Hello guys,
I am trying to boot my imx53-qsrb. I'm using a 4.0 kernel. I built u-boot, my kernel put the binaries on a fat16 partition of my Micro SD card. I downloaded a debian rootfs that I put it on the ext4 partition of my sd card. After booting my board here is the output :
| U-Boot 2015.04-dirty (May 11 2015 - 15:58:04) | ||
| Board: MX53 LOCO | ||
| I2C: ready | ||
| DRAM: 1 GiB | ||
| MMC: FSL_SDHC: 0, FSL_SDHC: 1 | ||
| In: | serial | |
| Out: serial | ||
| Err: serial | ||
| Net: FEC | ||
| Hit any key to stop autoboot: 0 | ||
| switch to partitions #0, OK | ||
| mmc0 is current device | ||
| SD/MMC found on device 0 | ||
| Checking for: /uEnv.txt ... | ||
| reading /uEnv.txt | ||
| 570 bytes read in 11 ms (49.8 KiB/s) | ||
| Loaded environment from /uEnv.txt | ||
| Checking if uenvcmd is set ... | ||
| Running uenvcmd ... | ||
| reading zImage | ||
| 5679310 bytes read in 115 ms (47.1 MiB/s) | ||
| ** No boot file defined ** | ||
| Kernel image @ 0x70010000 [ 0x000000 - 0x5653c0 ] | ||
Starting kernel ...
...
...
...
...
VFS: Cannot open root device "(null)" or unknown-block(0,0): error -6
Please append a correct "root=" boot option; here are the available partitions:
...
...
| b302 | 3837952 mmcblk0p2 b984de4c-02 |
| [ | 2.044505] Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0) | |
| [ | 2.052784] drm_kms_helper: panic occurred, switching back to text console | |
| [ | 2.060619] ---[ end Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0) |
[ 25.153014] random: nonblocking pool is initialized
Thanks
Hi Nabil
had you tried to add to kernel boot line
rootfstype=ext4
Best regards
igor
Hi Igor,
Yes, I did that, here is my uEnv.txt :
#u-boot mmc (SDcard) boot
kernel_file= zImage
#mmc (SDcard for bbb) parameters
mmcdev=0
mmcpart=1
loadzimage=load mmc ${mmcdev}:${mmcpart} ${loadaddr} ${kernel_file}
loadfdt=load mmc ${mmcdev}:${mmcpart} ${fdtaddr} ${fdtfile}
#systemd boot
optargs=quiet init=/hello_s.out
console=ttyO0,115200n8
mmcroot=/dev/mmcblk0p2 rw
mmcrootfstype=ext4 rootwait fixrtc
mmcargs=setenv bootargs console=${console} root=${mmcroot} rootfstype=${mmcrootfstype} ${optargs}
#boot commands for compressed image kernel
uenvcmd=run loadzimage; run loadfdt; run mmcargs; bootz ${loadaddr} - ${fdtaddr}
In the first partition mmcblk0p1 I have my uEnv.txt and my zImage (I used a zImage combined with th fdt). In the second partition mmcblk0p2 I have the my rootfs. I tried with both, debian and a hello_s.out file which is a hello_world statically compiled. I always got he same error.
Nabil