imx53 MFGtool error when using plugin-based U-Boot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx53 MFGtool error when using plugin-based U-Boot

1,341 次查看
bdp42
Contributor IV

We have an iMX53-based platform that uses the DCD approach in U-Boot to perform device configuring both for the production and manufacturing versions of U-Boot and we have been successfully using the Freescale MFGTool (using the manufacturing version of U-Boot) to program the boards.

We have now changed to use the plugin approach to configure the device for both production and manufacturing versions of U-Boot. The production U-Boot works and the board boots correctly. However the MFGTool fails straightway when attempting to program the board using the new plugin-based U-boot approach.

Does anyone know of any issues relating to the use the MFGTool when using the iMX53 plugin approach?

Does the xml file differ between the DCD and plugin approaches - we use the same xml file for both. I've attached a copy of the xml file.

The MfgTool version is V1.6.2.055.

Thanks

Bruno

Here's the relevant error from the MfgTool log

Monday, December 04, 2017 12:52:13
1 - Panel A Start processing BT500-V4 <LIST/>.

Panel A Start <CMD/> type="boot" body="BootStrap" file="u-boot-mfg.bin" timeout="10" onError="" text=" Boot from mfg-mode U-Boot ".

1 - Panel A DoBoot() - Failed to load u-boot-mfg.bin to Recovery mode device. (err=6)

1 - Panel A Finished <CMD/> type="boot" body="BootStrap" file="u-boot-mfg.bin" timeout="10" onError="" text=" Boot from mfg-mode U-Boot " FAIL code=0x6.

Panel A: Reason is unknown,failed to run command: type="boot" body="BootStrap" file="u-boot-mfg.bin" timeout="10" onError="" text=" Boot from mfg-mode U-Boot "  The handle is invalid.



2 - Panel A Finished processing BT500-V4 <LIST/> : FAIL code=6.

Panel A: Reason is unknown,Operation stopped by user. The process terminated unexpectedly.



标签 (1)
标记 (3)
0 项奖励
回复
1 回复

1,208 次查看
jimmychan
NXP TechSupport
NXP TechSupport

what is the meaning of "plugin" approach?

0 项奖励
回复