imx51 serial number

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,926件の閲覧回数
lukaszwysocki
Contributor I

Hello,

I have a problem with the imx51, I can not find in RM register where serial number is stored, can someone help me?

--

thx Lukasz

ラベル(3)
0 件の賞賛
返信
1 解決策
2,739件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

64bits unique id  addresses: 820-83c   Table 6-2. i.MX51 Fuse Map

http://www.freescale.com/files/dsp/doc/ref_manual/MCIMX51RM.pdf

Best regards

igor

元の投稿で解決策を見る

3 返答(返信)
2,740件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

64bits unique id  addresses: 820-83c   Table 6-2. i.MX51 Fuse Map

http://www.freescale.com/files/dsp/doc/ref_manual/MCIMX51RM.pdf

Best regards

igor

2,739件の閲覧回数
lukaszwysocki
Contributor I

Thank you very much!

--
Lukasz

0 件の賞賛
返信
2,739件の閲覧回数
BrilliantovKiri
Senior Contributor I

Hello, Lucasz!

Follow my code for iMX53:

/*

*  i.MX53 Applications Processor Reference Manual, Rev. 2.1, 5/2012

*  Table 2-10. Common Fusemap, p. 5088

*/

int cpu_id(unsigned int * __restrict m,

                        unsigned int * __restrict l)

{

        int fd = -1;

        unsigned char v[8] = {0}, i;

        fd = open("/dev/mxc_iim", O_RDONLY);

        if (fd <= 0)

                return -1;

        for (i = 0; i < 8; i++) {

                if (-1 == lseek(fd, 0x820 + i * 4, SEEK_SET))

                        goto ERROR;

                if (-1 == read(fd, &v[i], sizeof(char)))

                        goto ERROR;

        }

        close(fd);

        *m = (unsigned int)((v[0] << 24) | (v[1] << 16) |

                                                (v[2] << 8) | (v[3] << 0));

        *l = (unsigned int)((v[4] << 24) | (v[5] << 16) |

                                                (v[6] << 8) | (v[7] << 0));

        return 0;

ERROR:

        close(fd);

        return -1;

}

0 件の賞賛
返信