imx31 hardware interface - GPIOs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx31 hardware interface - GPIOs

3,955 Views
Olson
Contributor I
I am designing a system architecture with the imx31 while using the ADS as a reference. I am looking for a description of all the GPIO that I can have available to me through the functional multiplexing. Basically I need to know what GPIO I have available to me for interrupts. The documentation talks about having 32 GPIO through the GPIO module, but then the functional multiplexing and pinout charts show only 9 GPIO available (this seems very low), and anymore I cannot tell if they exist through multiplexing or not. Does anyone know how many independent GPIO I can use specifically for general purpose pins? Any help would be appreciated.
Tags (1)
0 Kudos
Reply
1 Reply

2,770 Views
Marcel_s
Contributor I
As far as I know you have 9. They are: GPIO1_0 -->GPIO1_6 and GPIO3_0 --> GPIO3_1

Are you working on a driver to control GPIO pins?

Rgds

Marcel
0 Kudos
Reply