imx287 gpio

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx287 gpio

3,614 次查看
adityapatil
Contributor II

I am working on imx287 CPU with linux-2.6.35.3.

I have configured the PIN 3_10 to be output and low in the kernel.

But, when I restart the pin remains high value till the kernel has initialized gpmi (mx28 pins) in file mx28evk_pins.c and then becomes low.

How can I avoid this and keep the pin low even after restart.

-Thanks

标记 (4)
0 项奖励
回复
4 回复数

3,291 次查看
adityapatil
Contributor II

hi igor,

I did some  modification in the file init-mx28.c in boot_prep of bootlet source code

//Pin_1_28 as out and low

HW_PINCTRL_MUXSEL3_SET(3 << 24);

HW_PINCTRL_DOE1_SET(1 << 24);

HW_PINCTRL_DOUT1_CLR(1 << 24);

But still the pin fails to be low on startup.

Thanks,

-Aditya

0 项奖励
回复

3,291 次查看
adityapatil
Contributor II

Hi

1.I have the bootlet sources

2. Can I add the gpio initialization in bootlet source without using ltib?

-Thanks

0 项奖励
回复

3,291 次查看
igorpadykov
NXP Employee
NXP Employee

in general one can use yocto with uboot, please look at

https://community.nxp.com/thread/306491 

~igor

0 项奖励
回复

3,291 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Aditya

one can add gpio initialization in bootlet sources.
For obtaining bootlets sources:

1. ./ltib -m prep -p imx-bootlets
This command will put imx-bootlets source codes in the folder --
ltib/rpm/build/

2. modify sources
3. ./ltib -m scbuild -p  imx-bootlets

This command will build new images.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------