imx287 - freertos

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx287 - freertos

2,824 次查看
ask
Contributor III

Hi,

Does anyone have a FreeRTOS port for imx287

Thanks for your time

0 项奖励
回复
3 回复数

2,440 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi,

If you refer to the “Software and Tools” tab of i.MX287 webpage, you can find some RTOS options like MQX, Nucleus and QNX; however, FreeRTOS is not available.

According with FreeRTOS webpage, i.MX28 is not listed on the Freescale supported devices; however, the RTOS for ARM9 could be adapted for the i.MX287.

There are other options for the migration, like third parties services (here is an example):


Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,440 次查看
TomE
Specialist II

This is the Coldfire Forum for MCFxxx parts. See if you can move your question to the i.MX forum:

i.MX Community

There should be a button or drop-down or something hidden somewhere that lets you move a post.

If you can find the "how do I use this forum forum" (used to be completely hidden) there may be an answer to that question there. That forum is here:

https://community.freescale.com/community/about

Tom

0 项奖励
回复

2,440 次查看
admin
Specialist II

Thanks Tom, I have moved the question to the i.MX Community

@ask please consider this general advice Where to post a Discussion? for better visibility.

Thank you for your interest in Freescale Community!

Denisse

0 项奖励
回复