imx287 GPIO default value

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx287 GPIO default value

1,594件の閲覧回数
adityapatil
Contributor II

hi, 

1. I am working on imx287 custom board using Linux-2.6.35.3

2. How can I keep the gpio value to be low by default.

3. After Restart my gpio are at high state 3.3v

-Thanks

Aditya

ラベル(2)
0 件の賞賛
返信
1 返信

1,466件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Aditya,

You can program the GPIO at the initialization of the board it takes minimun time. 

First you need to export the GPIO you want to test to the user space:

echo XX > /sys/class/gpio/export

XX shall be determined by the following algorithm:

GPIOA_[B] is the GPIO you want to export, where "A" is the GPIO bank and "B" is the offset of the pin in the bank. if the first available GPIO bank is 0 // (iMX.28, for example)     XX = A*32 + B; else // first GPIO bank is 1     XX = (A-1)*32 + B;

Regards