imx28 evk board - NFS mount and boot failure

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx28 evk board - NFS mount and boot failure

2,345件の閲覧回数
sureshbabu1z
Contributor I

Hello All,

I am facing problem while NFS mout and boot from TFTP Server and client.

Could you please help he I am unable to find problem where it is occurring.

1) I have set it up tftpboot and tftp service also i added.

 -> tftp loading image.

2) NFS

server(Host Linux ip) - 192.168.1.34

etc/exports -

/tmp/fs          *(rw,sync,subtree_check)
/tools/rootfs    *(rw,sync,subtree_check)

3) for NFS mounting

sudo mount -t nfs 192.168.1.34:/tools/rootfs  /tools/rootfs   -->?

the above mounting step is right or wrong.

otherwise please help me.

4) current printenv

MX28 U-Boot > printenv                                                          
bootcmd=run bootcmd_net                                                         
bootdelay=3                                                                     
baudrate=115200                                                                 
netmask=255.255.255.0                                                           
loadaddr=0x42000000                                                             
bootcmd_net=run bootargs_nfs; dhcp; bootm                                       
bootargs_mmc=setenv bootargs ${bootargs} root=/dev/mmcblk0p3 rw rootwait ip=dhc}
bootcmd_mmc=run bootargs_mmc; mmc read 0 ${loadaddr} 100 3000; bootm            
ethact=FEC0                                                                     
nfsroot=/tools/rootfs                                                           
bootargs_nfs=setenv bootargs ${bootargs} root=/dev/nfs ip=dhcp nfsroot=${server�
gatewayip=192.168.1.1                                                           
bootargs=console=ttyAM0,115200n8 root=/dev/nfs ip=dhcp nfsroot=192.168.1.101:/h�
bootfile=uImage                                                                 
ethaddr=00:04:9F:01:D2:E4                                                       
serverip=192.168.1.34                                                           
ipaddr=192.168.1.31                                                             
stdin=serial                                                                    
stdout=serial                                                                   
stderr=serial                                                                   
ver=U-Boot 2009.08 (Jul 05 2012 - 16:57:23)                                     
                                                                                
Environment size: 863/130044 bytes                                              
MX28 U-Boot >

5)

This is the message i am getting

U-Boot 2009.08 (Jul 05 2012 - 16:57:23)                                         
                                                                                
Freescale i.MX28 family                                                         
CPU:   454 MHz                                                                  
BUS:   151 MHz                                                                  
EMI:   205 MHz                                                                  
GPMI:   24 MHz                                                                  
DRAM:  128 MB                                                                   
MMC:   IMX_SSP_MMC: 0, IMX_SSP_MMC: 1                                           
In:    serial                                                                   
Out:   serial                                                                   
Err:   serial                                                                   
Net:   got MAC address from IIM: 00:04:9f:01:d2:e4                              
FEC0                                                                            
Hit any key to stop autoboot:  0                                                
** Too many args (max. 16) **                                                   
BOOTP broadcast 1                                                               
FEC: Link is down 7809                                                          
BOOTP broadcast 2                                                               
BOOTP broadcast 3                                                               
DHCP client bound to address 192.168.1.22                                       
Using FEC0 device                                                               
TFTP from server 192.168.1.34; our IP address is 192.168.1.22                   
Filename 'uImage'.                                                              
Load address: 0x42000000                                                        
Loading: #################################################################      
         #################################################################      
         #################################################################      
         #################################################################      
         #################################################################      
         #################################################################      
         #################################################################      
         ##############################################                         
done                                                                            
Bytes transferred = 2562288 (2718f0 hex)                                        
## Booting kernel from Legacy Image at 42000000 ...                             
   Image Name:   Linux-2.6.35.3-571-gcca29a0                                    
   Image Type:   ARM Linux Kernel Image (uncompressed)                          
   Data Size:    2562224 Bytes =  2.4 MB                                        
   Load Address: 40008000                                                       
   Entry Point:  40008000                                                       
   Verifying Checksum ... OK                                                    
   Loading Kernel Image ... OK                                                  
OK                                                                              
                                                                                
Starting kernel ...                                                             
                                                                                
Uncompressing Linux... done, booting the kernel.                                
Linux version 2.6.35.3-571-gcca29a0 (ivcbar049adm@ubuntu) (gcc version 4.4.4 (42
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177                   
CPU: VIVT data cache, VIVT instruction cache                                    
Machine: Freescale MX28EVK board                                                
Memory policy: ECC disabled, Data cache writeback                               
Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 32512      
Kernel command line: console=ttyAM0,115200n8 root=/dev/nfs ip=dhcp nfsroot=192.5
PID hash table entries: 512 (order: -1, 2048 bytes)                             
Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)                  
Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)                    
Memory: 128MB = 128MB total                                                     
Memory: 124316k/124316k available, 6756k reserved, 0K highmem                   
Virtual kernel memory layout:                                                   
    vector  : 0xffff0000 - 0xffff1000   (   4 kB)                               
    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)                               
    DMA     : 0xfde00000 - 0xffe00000   (  32 MB)                               
    vmalloc : 0xc8800000 - 0xf0000000   ( 632 MB)                               
    lowmem  : 0xc0000000 - 0xc8000000   ( 128 MB)                               
    modules : 0xbf000000 - 0xc0000000   (  16 MB)                               
      .init : 0xc0008000 - 0xc0030000   ( 160 kB)                               
      .text : 0xc0030000 - 0xc04f7000   (4892 kB)                               
      .data : 0xc04f8000 - 0xc0535960   ( 247 kB)                               
SLUB: Genslabs=11, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1         
Hierarchical RCU implementation.                                                
        RCU-based detection of stalled CPUs is disabled.                        
        Verbose stalled-CPUs detection is disabled.                             
NR_IRQS:288                                                                     
Console: colour dummy device 80x30                                              
console [ttyAM0] enabled                                                        
Calibrating delay loop... 226.09 BogoMIPS (lpj=1130496)                         
pid_max: default: 32768 minimum: 301                                            
Security Framework initialized                                                  
SELinux:  Initializing.                                                         
Mount-cache hash table entries: 512                                             
CPU: Testing write buffer coherency: ok                                         
regulator: core version 0.5                                                     
NET: Registered protocol family 16                                              
regulator: vddd: 800 <--> 1575 mV at 1500 mV fast normal                        
regulator: vdddbo: 800 <--> 1575 mV fast normal                                 
regulator: vdda: 1500 <--> 2275 mV at 1800 mV fast normal                       
vddio = 3380000, val=10                                                         
regulator: vddio: 2880 <--> 3680 mV at 3380 mV fast normal                      
regulator: overall_current: fast normal                                         
regulator: vbus5v:                                                              
regulator: mxs-duart-1: fast normal                                             
regulator: mxs-bl-1: fast normal                                                
regulator: mxs-i2c-1: fast normal                                               
regulator: mmc_ssp-1: fast normal                                               
regulator: mmc_ssp-2: fast normal                                               
regulator: charger-1: fast normal                                               
regulator: power-test-1: fast normal                                            
regulator: cpufreq-1: fast normal                                               
i.MX IRAM pool: 124 KB@0xc8820000                                               
Initializing GPMI pins                                                          
usb DR wakeup device is registered                                              
IMX usb wakeup probe                                                            
audit: cannot initialize inotify handle                                         
bio: create slab <bio-0> at 0                                                   
SCSI subsystem initialized                                                      
Freescale USB OTG Driver loaded, $Revision: 1.55 $                              
usbcore: registered new interface driver usbfs                                  
usbcore: registered new interface driver hub                                    
usbcore: registered new device driver usb                                       
Advanced Linux Sound Architecture Driver Version 1.0.23.                        
Switching to clocksource mxs clock source                                       
NET: Registered protocol family 2                                               
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)                  
TCP established hash table entries: 4096 (order: 3, 32768 bytes)                
TCP bind hash table entries: 4096 (order: 2, 16384 bytes)                       
TCP: Hash tables configured (established 4096 bind 4096)                        
TCP reno registered                                                             
UDP hash table entries: 256 (order: 0, 4096 bytes)                              
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)                         
NET: Registered protocol family 1                                               
RPC: Registered udp transport module.                                           
RPC: Registered tcp transport module.                                           
RPC: Registered tcp NFSv4.1 backchannel transport module.                       
Bus freq driver module loaded                                                   
IMX usb wakeup probe                                                            
usb h1 wakeup device is registered                                              
mxs_cpu_init: cpufreq init finished                                             
audit: initializing netlink socket (disabled)                                   
type=2000 audit(0.610:1): initialized                                           
VFS: Disk quotas dquot_6.5.2                                                    
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)                      
JFFS2 version 2.2. (NAND) �© 2001-2006 Red Hat, Inc.                            
msgmni has been set to 242                                                      
alg: No test for stdrng (krng)                                                  
cryptodev: driver loaded.                                                       
Block layer SCSI generic (bsg) driver version 0.4 loaded (major 253)            
io scheduler noop registered                                                    
io scheduler deadline registered                                                
io scheduler cfq registered (default)                                           
Console: switching to colour frame buffer device 100x30                         
mxs-duart.0: ttyAM0 at MMIO 0x80074000 (irq = 47) is a DebugUART                
mxs-auart.0: ttySP0 at MMIO 0x8006a000 (irq = 112) is a mxs-auart.0             
Found APPUART 3.1.0                                                             
mxs-auart.1: ttySP1 at MMIO 0x8006c000 (irq = 113) is a mxs-auart.1             
Found APPUART 3.1.0                                                             
mxs-auart.2: ttySP2 at MMIO 0x8006e000 (irq = 114) is a mxs-auart.2             
Found APPUART 3.1.0                                                             
mxs-auart.3: ttySP3 at MMIO 0x80070000 (irq = 115) is a mxs-auart.3             
Found APPUART 3.1.0                                                             
brd: module loaded                                                              
loop: module loaded                                                             
i.MX GPMI NFC                                                                   
NFC: Version 1, 8-chip GPMI and BCH                                             
Boot ROM: Version 1, Single-chip boot area, block mark swapping supported       
Scanning for NAND Flash chips...                                                
No NAND device found.                                                           
gpmi-nfc gpmi-nfc.0: Chip scan failed                                           
mxs-spi mxs-spi.0: Max possible speed 24000 = 24000000/2 kHz                    
mxs-spi mxs-spi.0: at 0x80014000 mapped to 0xF0014000, irq=84, bus 1, DMA ver_m4
FEC Ethernet Driver                                                             
fec_enet_mii_bus: probed                                                        
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver                      
fsl-ehci fsl-ehci: Freescale On-Chip EHCI Host Controller                       
fsl-ehci fsl-ehci: new USB bus registered, assigned bus number 1                
fsl-ehci fsl-ehci: irq 93, io base 0x80080000                                   
fsl-ehci fsl-ehci: USB 2.0 started, EHCI 1.00                                   
hub 1-0:1.0: USB hub found                                                      
hub 1-0:1.0: 1 port detected                                                    
fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller                     
fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 2              
fsl-ehci fsl-ehci.0: irq 92, io base 0x80090000                                 
fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00                                 
hub 2-0:1.0: USB hub found                                                      
hub 2-0:1.0: 1 port detected                                                    
Initializing USB Mass Storage driver...                                         
usbcore: registered new interface driver usb-storage                            
USB Mass Storage support registered.                                            
ARC USBOTG Device Controller driver (1 August 2005)                             
mice: PS/2 mouse device common for all mice                                     
input: mxs-kbd as /devices/platform/mxs-kbd.0/input/input0                      
input: MXS touchscreen as /devices/virtual/input/input1                         
MXS RTC driver v1.0 hardware v2.3.0                                             
mxs-rtc mxs-rtc.0: rtc core: registered mxs-rtc as rtc0                         
IR NEC protocol handler initialized                                             
IR RC5(x) protocol handler initialized                                          
IR RC6 protocol handler initialized                                             
IR JVC protocol handler initialized                                             
IR Sony protocol handler initialized                                            
Linux video capture interface: v2.00                                            
mxs-pxp mxs-pxp.0: initialized                                                  
mxs watchdog: initialized, heartbeat 19 sec                                     
mxs-mmc: MXS SSP Controller MMC Interface driver                                
mxs-mmc mxs-mmc.0: mmc0: MXS SSP MMC DMAIRQ 82 ERRIRQ 96                        
dcp dcp.0: DCP crypto enabled.!                                                 
usbcore: registered new interface driver hiddev                                 
usbcore: registered new interface driver usbhid                                 
usbhid: USB HID core driver                                                     
sgtl5000-i2c 0-000a: SGTL5000 revision 17                                       
mxs-spdif mxs-spdif.0: MXS SPDIF Audio Transmitter                              
No device for codec mxs spdif                                                   
No device for DAI mxs spdif                                                     
No device for DAI mxs-saif                                                      
No device for DAI mxs-spdif                                                     
asoc: SGTL5000 <-> mxs-saif mapping ok                                          
mmc0: new high speed SDHC card at address d555                                  
mmcblk0: mmc0:d555 SU04G 3.79 GiB                                               
 mmcblk0: p1 p2 p3                                                              
Failed to add route LINE_OUT->Ext Spk                                           
asoc: mxs spdif <-> mxs-spdif mapping ok                                        
ALSA device list:                                                               
  #0: mxs-evk (SGTL5000)                                                        
  #1: mxs-evk (mxs spdif)                                                       
TCP cubic registered                                                            
NET: Registered protocol family 17                                              
can: controller area network core (rev 20090105 abi 8)                          
NET: Registered protocol family 29                                              
can: raw protocol (rev 20090105)                                                
mxs-rtc mxs-rtc.0: setting system clock to 1970-01-01 00:59:04 UTC (3544)       
eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=0:00, irq=-1)    
eth1: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=0:01, irq=-1)    
Sending DHCP requests .                                                         
PHY: 0:00 - Link is Up - 100/Full                                               
.., OK                                                                          
IP-Config: Got DHCP answer from 0.0.0.0, my address is 192.168.1.31             
IP-Config: Complete:                                                            
     device=eth0, addr=192.168.1.31, mask=255.255.255.0, gw=192.168.1.1,        
     host=192.168.1.31, domain=ivcbar.local, nis-domain=(none),                 
     bootserver=0.0.0.0, rootserver=192.168.1.34, rootpath=                     
Looking up port of RPC 100003/2 on 192.168.1.34                                 
Looking up port of RPC 100005/1 on 192.168.1.34                                 
VFS: Mounted root (nfs filesystem) on device 0:14.                              
Freeing init memory: 160K                                                       
init started: BusyBox v1.15.0 ()                                                
starting pid 1113, tty '': '/etc/rc.d/rcS'                                      
Mounting /proc and /sys                                                         
Starting the hotplug events dispatcher udevd                                    
Synthesizing initial hotplug events                                             
Setting the hostname to freescale                                               
Mounting filesystems                                                            
Booted NFS, not relocating: /tmp /var                                           
ln: /etc/mtab: Permission denied                                                
mount: mounting usbfs on /proc/bus/usb failed: No such file or directory        
Running sysctl                                                                  
Setting up networking on loopback device:                                       
rm: cannot remove '/etc/resolv.conf': Permission denied                         
Setting up networking on eth0:                                                  
nfs: server 192.168.1.34 not responding, still trying                           

I have one IP address(192.168.1.31) but some it is showing some other ip address(192.168.1.22).

タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,217件の閲覧回数
Colin_MTData
Contributor III
Hello Suresh, You're getting further than I can with TFTP & NFS but I can help a little. 1) I'm not sure what this is. 2) Looks OK to me (but mine isn't working at all yet). Mine is more restrictive: /tools/rootfs 192.168.1.0/255.255.255.0(rw,no_root_squash,no_subtree_check,sync) NOTE: I think the "no_root_squash" will be important for you as root on the target will want root access to the rootfs tree (Check with someone who knows more about NFS) 3) This isn't needed (and if it is on your host server then it is wrong) It's the target machine that will eventually mount the host root directory as it's own root, not on /tools/rootfs 4)Notice that when the command bootargs_nfs is run ("bootargs_nfs=setenv bootargs ${bootargs} root=/de....") it will effectively append to bootargs each time. bootargs is supposed to be just "ttyAM0,115200n8" but your environment has been saved with bootargs as it is after the append and so when you boot it tries to add even more on to the end and exceeds 16 args. Set bootargs back to the correct string and saveenv again. 5)I'm envious I can't get this bit to work at all. My FEC0 isn't up. Your server (linux host) is 192.168.1.34. Some dhcp server (probably 192.168.1.34) is returning the 192.168.1.22 to the target when u-boot uses bootp/tftp to request an address. If you want to have a fixed address for your target I think you need to change the "ip=dhcp" to "ip=${ipaddr}" in the bootargs_nfs env. variable. (I'm not 100% sure because I can't get my ether net port up). After all that it still doesn't help you with your main problem of "nfs: server 192.168.1.34 not responding, still trying". I assume "/tools/rootfs" is where you have put the rootfs of the system. Colin
0 件の賞賛
返信

1,217件の閲覧回数
Colin_MTData
Contributor III
Hello Suresh, You're getting further than I can with TFTP & NFS but I can help a little. 1) I'm not sure what this is. 2) Look OK to me (but mine isn't working at all) 3) This isn't needed (and if it is on your host server then it is wrong) It's the target machine that will eventually mount the host root directory as it's own root, not on /tools/rootfs 4)Notice that when the command bootargs_nfs is run ("bootargs_nfs=setenv bootargs ${bootargs} root=/de....") it will effectively append to bootargs each time. bootargs is supposed to be just "ttyAM0,115200n8" but your environment has been saved with bootargs as it is after the append and so when you boot it tries to add even more on to the end and exceeds 16 args. Set bootargs back to the correct string and saveenv again. 5)I'm envious I can't get this bit to work at all. My FEC0 isn't up. Your server (linux host) is 192.168.1.34. Some dhcp server (probably 192.168.1.34) is returning the 192.168.1.22 to the target when u-boot uses bootp/tftp to request an address. If you want to have a fixed address for your target I think you need to change the "ip=dhcp" to "ip=${ipaddr}" in the bootargs_nfs env. variable. (I'm not 100% sure because I can't get my ether net port up). After all that it still doesn't help you with your main problem of "nfs: server 192.168.1.34 not responding, still trying". I assume "/tools/rootfs" is where you have put the rootfs of the system. Colin
0 件の賞賛
返信