Hello
I try to boot from nand flash. But I get an error.
Output form console:
0x80508002
0x80508002
I made the bootsream with the mxsboot tool.
nand dump from barebox:
md -s /dev/nand0
00000000: 00000000 00000000 00000000 fffffcd6 ................
00000010: 20424346 01000000 06193c50 00000000 FCB ....P<......
00000020: 00000800 00000840 00000040 00000000 ....@...@.......
00000030: 00000000 00000000 00000004 00000200 ................
00000040: 00000200 00000004 0000000a 00000003 ................
00000050: 00000000 00000000 00000000 00000000 ................
00000060: 00000000 00000000 00000000 00000000 ................
00000070: 00000000 00000200 00000400 00000200 ................
00000080: 00000200 00000100 000007cf 00000000 ................
00000090: 00000800 00000000 00000000 00000000 ................
000000a0: 00000000 00000000 00000000 00000000 ................
000000b0: 00000000 00000000 00000000 00000000 ................
000000c0: 00000000 00000000 00000000 00000000 ................
000000d0: 00000000 00000000 00000000 00000000 ................
000000e0: 00000000 00000000 00000000 00000000 ................
000000f0: 00000000 00000000 00000000 00000000 ................
We use a S34MS01 1Gb Spansion flash on our board.
I try to set ROM4 NAND_ROW_ADDRESS_BYTES to 2. But without succsess.
I can't understand why the system doesn't boot.
Have anybody a idea?
Thanks
Hi Peter
FSL does not support mxsboot, however one can try use
MFG Tool and link below
I.MX28_MFG_TOOL_LINUX
: Tool and documentation for downloading i.MX28 image during manufacturing.
Re: NAND device unrecognized with an Update Error 0xffffffea(-22)
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------