imx28 DUART

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx28 DUART

2,099 Views
weihuang
Contributor I

Hello all.

I designed my own PCB with a iMX28.I need to set up DUART baud rate,but I can't put the baud rate divisor written to the FBRD register(0X80074028).

So what can I do to resolve that ?

Many thanks in advance.

Labels (1)
0 Kudos
Reply
2 Replies

1,990 Views
Yuri
NXP Employee
NXP Employee

  Please use sources of the i.MX28 OBDS package as an example

how to init the DUART.

On-Board Diagnostic Suit for the i.MX28

i.MX287 Processors|Dual Ethernet|Freescale


Have a great day,
YUri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,990 Views
weihuang
Contributor I

It is of great help to me

regards

wei

0 Kudos
Reply