imx28 Battery Charger issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx28 Battery Charger issue

ソリューションへジャンプ
1,694件の閲覧回数
liyingchun
Contributor I

Hi expert

?I know that imx28 has a on chip battery charger and can charge the Li-ion battery. I want to know that if it can be used to charge the NI-MH battery ( nickel-metal hydride battery )?

I checked the AN4199 doc. It seems that it does not mention the related information.

Thanks very much!

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,565件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Basically it is possible to configure i.MX28 charger for Ni-MH,

but please take a look at the following general considerations.

  http://leakeem.hubpages.com/hub/Which-is-better-Nickel-Metal-Hydride-NiMH-or-Lithium-Ion-Li-ion-batt...


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,566件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Basically it is possible to configure i.MX28 charger for Ni-MH,

but please take a look at the following general considerations.

  http://leakeem.hubpages.com/hub/Which-is-better-Nickel-Metal-Hydride-NiMH-or-Lithium-Ion-Li-ion-batt...


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信