imx28 BSP source code (L2.6.35)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx28 BSP source code (L2.6.35)

4,393 Views
skt고객oh
Contributor I

Really Thanks,

but i am looking for "L2.6.35_10.12.01_SDK_source_bundle" is included "L2.6.35_10.12.01_SDK_docs.tar.gz", "L2.6.35_10.12.01_SDK_scripts.tar.gz" and "L2.6.35_10.12.01_SDK_source.tar.gz"

could you please let me know, where can i L2.6.35_10.12.01_SDK_source_bundle file?

Thanks.

0 Kudos
Reply
7 Replies

4,153 Views
kailas_kharse
Contributor IV

Hello,

I am also looking for  "L2.6.35_10.12.01_SDK_source_bundle file" can you please share it with me?

 

 

Thanks & Regards,

Kailas Kharse

0 Kudos
Reply

4,293 Views
Yuri
NXP Employee
NXP Employee

Hello,

  I forwarded You some links. Hope it helps.

Regards,

Yuri.

0 Kudos
Reply

2,684 Views
hassin
Contributor I
Hi Yuri Can you send me the Link as well , We are working with multiple imx chips [ varsicite boards e.g mx8m mx7 ] . we have an old product running at field with mx28 . I need the sources to use LTIB
0 Kudos
Reply

3,700 Views
mitsuhiro
Contributor I
Can you forward it to me? thank you
0 Kudos
Reply

3,997 Views
Junpapa
Contributor I

Can I have the same version ?

0 Kudos
Reply

4,200 Views
Andy740629
Contributor I

Could U give me 2.6.31 BSP ?

Thanks

 

0 Kudos
Reply

4,230 Views
526642524
Contributor I

Can you forward it to me? thank you

0 Kudos
Reply