imx28 5V Power supply patch

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx28 5V Power supply patch

1,319件の閲覧回数
bcstewart
Contributor III

Hi Yuri,

I also need this patch. 

What was the reason for it?

Brad

0 件の賞賛
返信
1 返信

1,244件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

L2.6.35_10.12_5V_SUPPLY_PATCH - Linux patch for i.MX28 SDK 2010.12 to add the most

robust support possible for a VDD5V or DCDC_BATT only configuration.

I've sent the patches via e-mail.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信