imx27 crystal specification

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx27 crystal specification

Jump to solution
3,222 Views
aurele
Contributor I

Hi,

I'm reviewing some piece of design around an IMX27, and I could not found the "Recommended External Crystal Specifications".

Does someone know where I could find this information?

as an example I found those kind of specification for IMX25 in this file : http://cache.freescale.com/files/dsp/doc/data_sheet/IMX25CEC.pdf?fr=gdc

but I could not find this information in IMX27 datasheets, maybe I missed a datasheet.

Thanks

Aurèle

Labels (1)
0 Kudos
Reply
1 Solution
3,073 Views
igorpadykov
NXP Employee
NXP Employee

26 MHz crystal requirements for IMX27 are te same as for i.MX25,

capacitance value for processor pin one can find in its ibis model.

View solution in original post

0 Kudos
Reply
4 Replies
3,073 Views
igorpadykov
NXP Employee
NXP Employee

Hi Traynard

i.MX27 documents have not such specs however one can use

i.MX25 specifications, they are valid for i.MX27 too.

I.MX processors share similar modules.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

3,073 Views
aurele
Contributor I

Thanks for your helpful answer,

Concerning the high frequency quartz, as it is different on both products (24MHz for IMX25 and 26MHz for IMX27), the usage can't be the same. please tell me if i'm wrong.

is it possible to get the internal capacitance value for oscilators pin on IMX27?

thanks for your help

0 Kudos
Reply
3,074 Views
igorpadykov
NXP Employee
NXP Employee

26 MHz crystal requirements for IMX27 are te same as for i.MX25,

capacitance value for processor pin one can find in its ibis model.

0 Kudos
Reply
3,073 Views
aurele
Contributor I

thanks for your fast answers

0 Kudos
Reply