imx27 bootstrap issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx27 bootstrap issue

2,195件の閲覧回数
zhangjay
Contributor II

Hi Everyone,

Where can I get imx27 bootstrap source code which run in imx27 processor?

Our own designed board has something wrong when programming image into flash.

Thanks anyway!

タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,956件の閲覧回数
Yuri
NXP Employee
NXP Employee

If You mean i.MX27 boot ROM sources - it is not available.

If the ATK is mentioned :

https://www.freescale.com/webapp/Download?colCode=IMX_ATK_SOURCE_CODE&appType=license&location=null

1,956件の閲覧回数
zhangjay
Contributor II

Dear Yuri,

Can you help me with this issue https://community.freescale.com/thread/310652

when execute the Bootstrap End Indication Operation, I got the error response(0x88888808), 0x88888888 is correct.


I don't know what the 88 88 88 08 meaning.

Can you help me?

0 件の賞賛
返信