imx25 internal RAM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,898件の閲覧回数
rbruce
Contributor II

I would like to load and execute a program in the imx25 internal RAM, either via the serial downloader or from SPI flash.  Is this possible?

I am assuming some portions of internal RAM are used by the ROM code and would be off limits.  I don't find much information on internal RAM in the imx25 reference manual.

ラベル(1)
0 件の賞賛
返信
1 解決策
3,752件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hope the enclosed example helps.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,753件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hope the enclosed example helps.

0 件の賞賛
返信
3,747件の閲覧回数
rbruce
Contributor II

OK. I’m running a small program from internal RAM based on the sample you sent .

Thanks very much for your help.

Robert W. (Bill) Bruce

Watlow

Winona, MN

0 件の賞賛
返信
3,747件の閲覧回数
rbruce
Contributor II

Yuri,

Thanks for the example. After a quick look at the files, I think this will help me accomplish what I want to do.

Robert W.(Bill) Bruce

Watlow

Winona, MN

0 件の賞賛
返信