imx25 internal RAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx25 internal RAM

Jump to solution
2,895 Views
rbruce
Contributor II

I would like to load and execute a program in the imx25 internal RAM, either via the serial downloader or from SPI flash.  Is this possible?

I am assuming some portions of internal RAM are used by the ROM code and would be off limits.  I don't find much information on internal RAM in the imx25 reference manual.

Labels (1)
0 Kudos
Reply
1 Solution
2,749 Views
Yuri
NXP Employee
NXP Employee

Hope the enclosed example helps.

View solution in original post

0 Kudos
Reply
3 Replies
2,750 Views
Yuri
NXP Employee
NXP Employee

Hope the enclosed example helps.

0 Kudos
Reply
2,744 Views
rbruce
Contributor II

OK. I’m running a small program from internal RAM based on the sample you sent .

Thanks very much for your help.

Robert W. (Bill) Bruce

Watlow

Winona, MN

0 Kudos
Reply
2,744 Views
rbruce
Contributor II

Yuri,

Thanks for the example. After a quick look at the files, I think this will help me accomplish what I want to do.

Robert W.(Bill) Bruce

Watlow

Winona, MN

0 Kudos
Reply