imx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 
1,327 Views
ankitsoni
Contributor I

sir

 

we are working on  IMX6q - SABRESD board and the sample images with the product working properly.

then we downloaded LTIB and start building the kernel according to our requirement. and we are trying to load the uImage alone throgh tftp server (it is loading properly).

but it is failing during booting with a last mesege  and device is shutting down after 3 to 4 second.

=========================================================

EXT3-fs (mmcblk0p2): warning: maximal mount count reached, running e2fsck is recommended

EXT3-fs (mmcblk0p2): using internal journal

EXT3-fs (mmcblk0p2): recovery complete

EXT3-fs (mmcblk0p2): mounted filesystem with writeback data mode

VFS: Mounted root (ext3 filesystem) on device 179:2.

Freeing init memory: 208K

====================================================

 

i have couple of questions regarding to these

 

1.any problem with environment variables i set

2.how to load the root file system  when image is loading through tftp.

 

we are using one linux loaded SD card for uboot an all.(YOCTO project sample )

i attached the boot log and environment variables.

Original Attachment has been moved to: boot.txt.zip

Original Attachment has been moved to: env.txt.zip

0 Kudos
Reply
1 Solution
1,151 Views
b36401
NXP Employee
NXP Employee

Please doublecheck what do you mean failing?

The log you attached (boot.txt) looks fine.

And I see there this login prompt

imx6qdlsolo login:

near the end of the log.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,152 Views
b36401
NXP Employee
NXP Employee

Please doublecheck what do you mean failing?

The log you attached (boot.txt) looks fine.

And I see there this login prompt

imx6qdlsolo login:

near the end of the log.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply