imx-gpu-sdk_5.5.3.bb:do_compile) failed with exit code '1'

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx-gpu-sdk_5.5.3.bb:do_compile) failed with exit code '1'

848 次查看
qin1
Contributor I

ERROR: imx-gpu-sdk-5.5.3-r0 do_compile: Execution of '/work/imx8_linux_project/imx-yocto-bsp/imx8qxpc0mek_wayland/tmp/work/aarch64-mx8-poky-linux/imx-gpu-sdk/5.5.3-r0/temp/run.do_compile.752' failed with exit code 1:
PlatformName: Yocto
WARNING: Environment variable FSL_GRAPHICS_SDK_THIRD_PARTY_LIBS_DIR was not defined, so we force defined it.
Its highly recommended to manually define this variable so you can reuse the thirdparty libs between builds and repositories.
Read DocBuildingExternals.md for detailed information about this environment variable.
FSL_GRAPHICS_SDK=/work/imx8_linux_project/imx-yocto-bsp/imx8qxpc0mek_wayland/tmp/work/aarch64-mx8-poky-linux/imx-gpu-sdk/5.5.3-r0/git
FSL_GRAPHICS_SDK_ANDROID_PROJECT_DIR=/work/imx8_linux_project/imx-yocto-bsp/imx8qxpc0mek_wayland/tmp/work/aarch64-mx8-poky-linux/imx-gpu-sdk/5.5.3-r0/git/Android
FSL_GRAPHICS_SDK_THIRD_PARTY_LIBS_DIR=/work/imx8_linux_project/imx-yocto-bsp/imx8qxpc0mek_wayland/tmp/work/aarch64-mx8-poky-linux/imx-gpu-sdk/5.5.3-r0/git/.Thirdparty
ROOTFS=/work/imx8_linux_project/imx-yocto-bsp/imx8qxpc0mek_wayland/tmp/work/aarch64-mx8-poky-linux/imx-gpu-sdk/5.5.3-r0/recipe-sysroot
Traceback (most recent call last):
File "/work/imx8_linux_project/imx-yocto-bsp/imx8qxpc0mek_wayland/tmp/work/aarch64-mx8-poky-linux/imx-gpu-sdk/5.5.3-r0/git/.Config/FslBuild.py", line 38, in <module>
from FslBuildGen.Tool.Flow.ToolFlowBuild import ToolAppFlowFactory
File "/work/imx8_linux_project/imx-yocto-bsp/imx8qxpc0mek_wayland/tmp/work/aarch64-mx8-poky-linux/imx-gpu-sdk/5.5.3-r0/git/.Config/FslBuildGen/Tool/Flow/ToolFlowBuild.py", line 39, in <module>
from FslBuildGen import Main as MainFlow
File "/work/imx8_linux_project/imx-yocto-bsp/imx8qxpc0mek_wayland/tmp/work/aarch64-mx8-poky-linux/imx-gpu-sdk/5.5.3-r0/git/.Config/FslBuildGen/Main.py", line 49, in <module>
from FslBuildGen.Build.Filter import PackageFilter
File "/work/imx8_linux_project/imx-yocto-bsp/imx8qxpc0mek_wayland/tmp/work/aarch64-mx8-poky-linux/imx-gpu-sdk/5.5.3-r0/git/.Config/FslBuildGen/Build/Filter.py", line 43, in <module>
from FslBuildGen.Build.RequirementTree import RequirementTree
File "/work/imx8_linux_project/imx-yocto-bsp/imx8qxpc0mek_wayland/tmp/work/aarch64-mx8-poky-linux/imx-gpu-sdk/5.5.3-r0/git/.Config/FslBuildGen/Build/RequirementTree.py", line 38, in <module>
from FslBuildGen.Build import RequirementTreeUtil
File "/work/imx8_linux_project/imx-yocto-bsp/imx8qxpc0mek_wayland/tmp/work/aarch64-mx8-poky-linux/imx-gpu-sdk/5.5.3-r0/git/.Config/FslBuildGen/Build/RequirementTreeUtil.py", line 71, in <module>
qualifiedExtensionNameList: ExtensionListManager) -> None:
File "/usr/lib/python3.5/typing.py", line 1187, in overload
raise RuntimeError("Overloading is only supported in library stubs")
RuntimeError: Overloading is only supported in library stubs
WARNING: /work/imx8_linux_project/imx-yocto-bsp/imx8qxpc0mek_wayland/tmp/work/aarch64-mx8-poky-linux/imx-gpu-sdk/5.5.3-r0/temp/run.do_compile.752:1 exit 1 from 'FslBuild.py -vvvvv -t sdk --UseFeatures [EGL,EarlyAccess,OpenVG,G2D,OpenGLES2,OpenCV,Vulkan,OpenGLES3,OpenGLES3.1,OpenCL,OpenCL1.1,OpenCL1.2,OpenVX,OpenVX1.1] --UseExtensions [*] --Variants [WindowSystem=Wayland] --BuildThreads 4 -c install --CMakeInstallPrefix /work/imx8_linux_project/imx-yocto-bsp/imx8qxpc0mek_wayland/tmp/work/aarch64-mx8-poky-linux/imx-gpu-sdk/5.5.3-r0/git'

ERROR: Logfile of failure stored in: /work/imx8_linux_project/imx-yocto-bsp/imx8qxpc0mek_wayland/tmp/work/aarch64-mx8-poky-linux/imx-gpu-sdk/5.5.3-r0/temp/log.do_compile.752

Log data follows:
| DEBUG: Executing shell function do_compile
| PlatformName: Yocto
| WARNING: Environment variable FSL_GRAPHICS_SDK_THIRD_PARTY_LIBS_DIR was not defined, so we force defined it.
| Its highly recommended to manually define this variable so you can reuse the thirdparty libs between builds and repositories.
| Read DocBuildingExternals.md for detailed information about this environment variable.
| FSL_GRAPHICS_SDK=/work/imx8_linux_project/imx-yocto-bsp/imx8qxpc0mek_wayland/tmp/work/aarch64-mx8-poky-linux/imx-gpu-sdk/5.5.3-r0/git
| FSL_GRAPHICS_SDK_ANDROID_PROJECT_DIR=/work/imx8_linux_project/imx-yocto-bsp/imx8qxpc0mek_wayland/tmp/work/aarch64-mx8-poky-linux/imx-gpu-sdk/5.5.3-r0/git/Android
| FSL_GRAPHICS_SDK_THIRD_PARTY_LIBS_DIR=/work/imx8_linux_project/imx-yocto-bsp/imx8qxpc0mek_wayland/tmp/work/aarch64-mx8-poky-linux/imx-gpu-sdk/5.5.3-r0/git/.Thirdparty
| ROOTFS=/work/imx8_linux_project/imx-yocto-bsp/imx8qxpc0mek_wayland/tmp/work/aarch64-mx8-poky-linux/imx-gpu-sdk/5.5.3-r0/recipe-sysroot
| Traceback (most recent call last):
| File "/work/imx8_linux_project/imx-yocto-bsp/imx8qxpc0mek_wayland/tmp/work/aarch64-mx8-poky-linux/imx-gpu-sdk/5.5.3-r0/git/.Config/FslBuild.py", line 38, in <module>
| from FslBuildGen.Tool.Flow.ToolFlowBuild import ToolAppFlowFactory
| File "/work/imx8_linux_project/imx-yocto-bsp/imx8qxpc0mek_wayland/tmp/work/aarch64-mx8-poky-linux/imx-gpu-sdk/5.5.3-r0/git/.Config/FslBuildGen/Tool/Flow/ToolFlowBuild.py", line 39, in <module>
| from FslBuildGen import Main as MainFlow
| File "/work/imx8_linux_project/imx-yocto-bsp/imx8qxpc0mek_wayland/tmp/work/aarch64-mx8-poky-linux/imx-gpu-sdk/5.5.3-r0/git/.Config/FslBuildGen/Main.py", line 49, in <module>
| from FslBuildGen.Build.Filter import PackageFilter
| File "/work/imx8_linux_project/imx-yocto-bsp/imx8qxpc0mek_wayland/tmp/work/aarch64-mx8-poky-linux/imx-gpu-sdk/5.5.3-r0/git/.Config/FslBuildGen/Build/Filter.py", line 43, in <module>
| from FslBuildGen.Build.RequirementTree import RequirementTree
| File "/work/imx8_linux_project/imx-yocto-bsp/imx8qxpc0mek_wayland/tmp/work/aarch64-mx8-poky-linux/imx-gpu-sdk/5.5.3-r0/git/.Config/FslBuildGen/Build/RequirementTree.py", line 38, in <module>
| from FslBuildGen.Build import RequirementTreeUtil
| File "/work/imx8_linux_project/imx-yocto-bsp/imx8qxpc0mek_wayland/tmp/work/aarch64-mx8-poky-linux/imx-gpu-sdk/5.5.3-r0/git/.Config/FslBuildGen/Build/RequirementTreeUtil.py", line 71, in <module>
| qualifiedExtensionNameList: ExtensionListManager) -> None:
| File "/usr/lib/python3.5/typing.py", line 1187, in overload
| raise RuntimeError("Overloading is only supported in library stubs")
| RuntimeError: Overloading is only supported in library stubs
| WARNING: /work/imx8_linux_project/imx-yocto-bsp/imx8qxpc0mek_wayland/tmp/work/aarch64-mx8-poky-linux/imx-gpu-sdk/5.5.3-r0/temp/run.do_compile.752:1 exit 1 from 'FslBuild.py -vvvvv -t sdk --UseFeatures [EGL,EarlyAccess,OpenVG,G2D,OpenGLES2,OpenCV,Vulkan,OpenGLES3,OpenGLES3.1,OpenCL,OpenCL1.1,OpenCL1.2,OpenVX,OpenVX1.1] --UseExtensions [*] --Variants [WindowSystem=Wayland] --BuildThreads 4 -c install --CMakeInstallPrefix /work/imx8_linux_project/imx-yocto-bsp/imx8qxpc0mek_wayland/tmp/work/aarch64-mx8-poky-linux/imx-gpu-sdk/5.5.3-r0/git'
| ERROR: Execution of '/work/imx8_linux_project/imx-yocto-bsp/imx8qxpc0mek_wayland/tmp/work/aarch64-mx8-poky-linux/imx-gpu-sdk/5.5.3-r0/temp/run.do_compile.752' failed with exit code 1:
| PlatformName: Yocto
| WARNING: Environment variable FSL_GRAPHICS_SDK_THIRD_PARTY_LIBS_DIR was not defined, so we force defined it.
| Its highly recommended to manually define this variable so you can reuse the thirdparty libs between builds and repositories.
| Read DocBuildingExternals.md for detailed information about this environment variable.
| FSL_GRAPHICS_SDK=/work/imx8_linux_project/imx-yocto-bsp/imx8qxpc0mek_wayland/tmp/work/aarch64-mx8-poky-linux/imx-gpu-sdk/5.5.3-r0/git
| FSL_GRAPHICS_SDK_ANDROID_PROJECT_DIR=/work/imx8_linux_project/imx-yocto-bsp/imx8qxpc0mek_wayland/tmp/work/aarch64-mx8-poky-linux/imx-gpu-sdk/5.5.3-r0/git/Android
| FSL_GRAPHICS_SDK_THIRD_PARTY_LIBS_DIR=/work/imx8_linux_project/imx-yocto-bsp/imx8qxpc0mek_wayland/tmp/work/aarch64-mx8-poky-linux/imx-gpu-sdk/5.5.3-r0/git/.Thirdparty
| ROOTFS=/work/imx8_linux_project/imx-yocto-bsp/imx8qxpc0mek_wayland/tmp/work/aarch64-mx8-poky-linux/imx-gpu-sdk/5.5.3-r0/recipe-sysroot
| Traceback (most recent call last):
| File "/work/imx8_linux_project/imx-yocto-bsp/imx8qxpc0mek_wayland/tmp/work/aarch64-mx8-poky-linux/imx-gpu-sdk/5.5.3-r0/git/.Config/FslBuild.py", line 38, in <module>
| from FslBuildGen.Tool.Flow.ToolFlowBuild import ToolAppFlowFactory
| File "/work/imx8_linux_project/imx-yocto-bsp/imx8qxpc0mek_wayland/tmp/work/aarch64-mx8-poky-linux/imx-gpu-sdk/5.5.3-r0/git/.Config/FslBuildGen/Tool/Flow/ToolFlowBuild.py", line 39, in <module>
| from FslBuildGen import Main as MainFlow
| File "/work/imx8_linux_project/imx-yocto-bsp/imx8qxpc0mek_wayland/tmp/work/aarch64-mx8-poky-linux/imx-gpu-sdk/5.5.3-r0/git/.Config/FslBuildGen/Main.py", line 49, in <module>
| from FslBuildGen.Build.Filter import PackageFilter
| File "/work/imx8_linux_project/imx-yocto-bsp/imx8qxpc0mek_wayland/tmp/work/aarch64-mx8-poky-linux/imx-gpu-sdk/5.5.3-r0/git/.Config/FslBuildGen/Build/Filter.py", line 43, in <module>
| from FslBuildGen.Build.RequirementTree import RequirementTree
| File "/work/imx8_linux_project/imx-yocto-bsp/imx8qxpc0mek_wayland/tmp/work/aarch64-mx8-poky-linux/imx-gpu-sdk/5.5.3-r0/git/.Config/FslBuildGen/Build/RequirementTree.py", line 38, in <module>
| from FslBuildGen.Build import RequirementTreeUtil
| File "/work/imx8_linux_project/imx-yocto-bsp/imx8qxpc0mek_wayland/tmp/work/aarch64-mx8-poky-linux/imx-gpu-sdk/5.5.3-r0/git/.Config/FslBuildGen/Build/RequirementTreeUtil.py", line 71, in <module>
| qualifiedExtensionNameList: ExtensionListManager) -> None:
| File "/usr/lib/python3.5/typing.py", line 1187, in overload
| raise RuntimeError("Overloading is only supported in library stubs")
| RuntimeError: Overloading is only supported in library stubs
| WARNING: /work/imx8_linux_project/imx-yocto-bsp/imx8qxpc0mek_wayland/tmp/work/aarch64-mx8-poky-linux/imx-gpu-sdk/5.5.3-r0/temp/run.do_compile.752:1 exit 1 from 'FslBuild.py -vvvvv -t sdk --UseFeatures [EGL,EarlyAccess,OpenVG,G2D,OpenGLES2,OpenCV,Vulkan,OpenGLES3,OpenGLES3.1,OpenCL,OpenCL1.1,OpenCL1.2,OpenVX,OpenVX1.1] --UseExtensions [*] --Variants [WindowSystem=Wayland] --BuildThreads 4 -c install --CMakeInstallPrefix /work/imx8_linux_project/imx-yocto-bsp/imx8qxpc0mek_wayland/tmp/work/aarch64-mx8-poky-linux/imx-gpu-sdk/5.5.3-r0/git'
|
ERROR: Task (/work/imx8_linux_project/imx-yocto-bsp/sources/meta-imx/meta-sdk/recipes-graphics/imx-gpu-sdk/imx-gpu-sdk_5.5.3.bb:do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 4317 tasks of which 4314 didn't need to be rerun and 1 failed.

0 项奖励
回复
0 回复数