imx glClearColor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx glClearColor

1,477件の閲覧回数
jjordan
Contributor I

I am using a custom board (with custom screen) on an imx535. I am trying to use some of the gles 2.0 frame buffer samples in the gpusdk. One of the problems I am running into is that glClearColor always seems to only show red (when it shows anything). I started with lesson02 but have seen the problem on the es20/lesson05/lesson05_imx.c as well. I have added some glut code so I could test it on my desktop, which does show the correct color. I thought it might be something in my egl config, but I tried all that are available and saw no change.

 

I have attached the file I am using. Thanks for your help

Original Attachment has been moved to: lesson05_imx.c.txt.zip

ラベル(3)
0 件の賞賛
返信
1 返信

1,338件の閲覧回数
ChucoChe
NXP Employee
NXP Employee

Hi,

Are you able to run simpletriangle or tiger? They are both in /usr/bin.

Michel

0 件の賞賛
返信