imx docker - imx nano 8 - compiling fails

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx docker - imx nano 8 - compiling fails

497 次查看
xavgru
Contributor I

Using release imx-6.6.52-2.2.0 and imx 8 nano, compiling fails:

bitbake imx-image-core

 

compiling minimal also fails:

bitbake core-image-minimal

 

error:
ERROR: core-image-minimal-1.0-r0 do_rootfs: The postinstall intercept hook 'update_desktop_database' failed, details in /opt/yocto/imx-6.6.52-2.2.0-build/build_fsl-imx-xwayland/tmp/work/imx8mnevk-poky-linux/core-image-minimal/1.0/temp/log.do_rootfs
ERROR: Logfile of failure stored in: /opt/yocto/imx-6.6.52-2.2.0-build/build_fsl-imx-xwayland/tmp/work/imx8mnevk-poky-linux/core-image-minimal/1.0/temp/log.do_rootfs.3164302
ERROR: Task (/opt/yocto/imx-6.6.52-2.2.0-build/sources/poky/meta/recipes-core/images/core-image-minimal.bb:do_rootfs) failed with exit code '1'

complete log:
https://gist.github.com/xavgru12/ae9620cd9b4221787c3d4ff42502b9b7

0 项奖励
回复
1 回复

483 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Could you share the steps you have followed for building so I can double check on my side?

Best regards/Saludos,
Aldo.

0 项奖励
回复