imx cpufreq setting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx cpufreq setting

2,904件の閲覧回数
brkantor
Contributor I

I work on lowering of imx28 power consumption.

I seemed, there are available frequencies: 454, 360 and 261MHz.

Is it possible to use 64MHz mentioned in imx28 documentation?

 

BTW

How about cpuidle?

Are there any plans to use it on imx28?

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,489件の閲覧回数
TimWoodham
Contributor I
I've found it is possible with mDDR ram.
0 件の賞賛
返信

2,489件の閲覧回数
AhmetYUCE
Contributor II
CPU Idle is available and working on iMX8, just turn it on in the kernel settings. Regarding CPUFreq, there is a bug in BSP or silicon issue. Changing CPU core freq to 454,360 and 261MHz not a problem. But in parallel CPUFreq driver also changes EMI freq into 200,166 and 133MHz, which leads to lockup. 200MHz EMI for all three core freq is safe and working. 133MHz definitely not working. 166Mhz, well it depends. Just check out the discussion i've started few months ago. Regards Ahmet
0 件の賞賛
返信

2,489件の閲覧回数
PavelNakonechny
Contributor I

There is mistake in cpufreq.c with calculation of variables lcd_on_freq_table_size and lcd_off_freq_table_size.

 

Fix them accordingly for your board, and enjoy minimal frequency. This works for our board based on i.MX287:

lcd_on_freq_table_size = ARRAY_SIZE(profiles);
lcd_off_freq_table_size = ARRAY_SIZE(profiles);

:-)

0 件の賞賛
返信