imx config tool ddr tool

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx config tool ddr tool

492件の閲覧回数
stoemarc
Contributor III

Hello, I get stuck at reset target. I’m not using PMIC, is this issue due to PMIC? I selected inside config tool DDR config → Board Configuration → PMIC initialization disabled

#################### Result for: phy_init ###### Run 1 #############################################Microsoft Windows [Version 10.0.22631.5189]
(c) Microsoft Corporation. All rights reserved.

C:\nxp\i.MX_CFG_25.03\bin>prompt test-prefix :

test-prefix : “C:/nxp/i.MX_CFG_25.03/bin/python3/python” “C:/nxp/i.MX_CFG_25.03/bin/python3/memtool/memtool_entry.py” -t “runtest” -d “C:/ProgramData/NXP/mcu_data_25.03/processors/MIMX9596xxxxQ/ksdk2_0/mem_validation/ddrc” -p “C:/Users//AppData/Local/Temp/mem_validation/phy_training_phy_test_0_0_.log” -l INFO “C:/Users//AppData/Local/Temp/mem_validation/connect.json” “C:/Users//AppData/Local/Temp/mem_validation/test.json” “C:/Users//AppData/Local/Temp/mem_validation/phy.json” “C:/Users//AppData/Local/Temp/mem_validation/ddrc_registers.json” “C:/Users//AppData/Local/Temp/mem_validation/ddrc_config.json” “C:/Users/163055~1/AppData/Local/Temp/mem_validation/ddrc_config_in.json”
INFO memtool.utils.helper *****C:/Users//AppData/Local/Temp/mem_validation/connect.json
INFO memtool.utils.helper *****C:/Users//AppData/Local/Temp/mem_validation/test.json
INFO memtool.utils.helper *****C:/Users//AppData/Local/Temp/mem_validation/phy.json
INFO memtool.utils.helper *****C:/Users//AppData/Local/Temp/mem_validation/ddrc_registers.json
INFO memtool.utils.helper *****C:/Users//AppData/Local/Temp/mem_validation/ddrc_config.json
INFO memtool.utils.helper *****C:/Users//AppData/Local/Temp/mem_validation/ddrc_config_in.json
INFO memtool.processor.imx9.imx9_processor Xls mapping load time 0.052813
INFO memtool.processor.imx9.imx9_processor Config time 0.000317
INFO memtool.processor.imx9.imx9_processor DS file time 0.359792
INFO memtool.phyinit.phy_init Run phyinit for 2024.09\lpddr5
INFO memtool.comm.serial_channel Using serial: COM3
INFO memtool.comm.serial_channel Send reset to target

0 件の賞賛
返信
1 返信

438件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

If you are using a custom configuration, please check the next:

- If you use a different debug UART port as NXP EVK does, you must configure debug UART IOMUX and debug port in the beginning of the DDR script according to your schematics.

- If you are not using a PMIC in your design, you need to skip the PMIC initialization, but you need to verify that the board is following the power up sequence of i.MX95.

Best regards.

0 件の賞賛
返信