imx-boot not find when build embedded linux on imx8mplus with yocto

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx-boot not find when build embedded linux on imx8mplus with yocto

2,504 次查看
arash_eng
Contributor I

 

Hi, I tried to build embedded linux with the help of Yocto for the imx8mplus evaluation board but when bitbake wants to deploy image file I received the error that shows the imx-boot file doesn't find.

 

 

Loading cache: 100% |############################################| Time: 0:00:00
Loaded 4736 entries from dependency cache.
Parsing recipes: 100% |##########################################| Time: 0:00:02
Parsing of 3190 .bb files complete (3188 cached, 2 parsed). 4738 targets, 527 skipped, 3 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION = "2.0.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "universal"
TARGET_SYS = "aarch64-poky-linux"
MACHINE = "imx8mp-lpddr4-evk"
DISTRO = "fsl-imx-wayland"
DISTRO_VERSION = "5.15-kirkstone"
TUNE_FEATURES = "aarch64 armv8a crc crypto"
TARGET_FPU = ""
meta
meta-poky = "HEAD:24a3f7b3648185e33133f5d96b184a6cb6524f3d"
meta-oe
meta-multimedia
meta-python = "HEAD:744a4b6eda88b9a9ca1cf0df6e18be384d9054e3"
meta-freescale = "HEAD:c82d4634e7aba8bc0de73ce1dfc997b630051571"
meta-freescale-3rdparty = "HEAD:5977197340c7a7db17fe3e02a4e014ad997565ae"
meta-freescale-distro = "HEAD:d5bbb487b2816dfc74984a78b67f7361ce404253"
meta-bsp
meta-sdk
meta-ml
meta-v2x = "HEAD:01df9917808c12ac561b417d2b1f3652a64cdab9"
meta-nxp-demo-experience = "HEAD:52eaf8bf42f8eda2917a1c8c046003c8c2c8f629"
meta-chromium = "HEAD:e232c2e21b96dc092d9af8bea4b3a528e7a46dd6"
meta-clang = "HEAD:c728c3f9168c8a4ed05163a51dd48ca1ad8ac21d"
meta-gnome
meta-networking
meta-filesystems = "HEAD:744a4b6eda88b9a9ca1cf0df6e18be384d9054e3"
meta-qt6 = "HEAD:ed785a25d12e365d1054700d4fc94a053176eb14"
meta-virtualization = "HEAD:9482648daf0bb42ff3475e7892542cf99f3b8d48"

WARNING: /home/arash/Desktop/imx-yocto-bsp/sources/meta-imx/meta-ml/recipes-libraries/tensorflow-lite/tensorflow-lite-vx-delegate_2.9.1.bb:do_compile is tainted from a forced run
Initialising tasks: 100% |#######################################| Time: 0:00:06
Sstate summary: Wanted 21 Local 19 Mirrors 0 Missed 2 Current 4260 (90% match, 99% complete)
NOTE: Executing Tasks
ERROR: imx-image-full-1.0-r0 do_image_wic: ExecutionError('/home/arash/Desktop/imx-yocto-bsp/build-wayland/tmp/work/imx8mp_lpddr4_evk-poky-linux/imx-image-full/1.0-r0/temp/run.do_image_wic.4068', 1, None, None)
ERROR: Logfile of failure stored in: /home/arash/Desktop/imx-yocto-bsp/build-wayland/tmp/work/imx8mp_lpddr4_evk-poky-linux/imx-image-full/1.0-r0/temp/log.do_image_wic.4068
Log data follows:
| DEBUG: Executing python function extend_recipe_sysroot
| NOTE: Direct dependencies are ['/home/arash/Desktop/imx-yocto-bsp/sources/meta-imx/meta-bsp/recipes-bsp/imx-mkimage/imx-boot_1.0.bb:do_populate_sysroot', '/home/arash/Desktop/imx-yocto-bsp/sources/meta-imx/meta-bsp/recipes-bsp/u-boot/u-boot-imx_2022.04.bb:do_populate_sysroot', '/home/arash/Desktop/imx-yocto-bsp/sources/meta-imx/meta-bsp/recipes-fsl/mcore-demos/imx-m7-demos_2.12.1.bb:do_populate_sysroot', '/home/arash/Desktop/imx-yocto-bsp/sources/poky/meta/recipes-core/glibc/cross-localedef-native_2.35.bb:do_populate_sysroot', '/home/arash/Desktop/imx-yocto-bsp/sources/poky/meta/recipes-core/glibc/ldconfig-native_2.12.1.bb:do_populate_sysroot', '/home/arash/Desktop/imx-yocto-bsp/sources/poky/meta/recipes-devtools/qemu/qemuwrapper-cross_1.0.bb:do_populate_sysroot', '/home/arash/Desktop/imx-yocto-bsp/sources/poky/meta/recipes-kernel/kmod/depmodwrapper-cross_1.0.bb:do_populate_sysroot', 'virtual:native:/home/arash/Desktop/imx-yocto-bsp/sources/poky/meta/recipes-core/update-rc.d/update-rc.d_0.8.bb:do_populate_sysroot', 'virtual:native:/home/arash/Desktop/imx-yocto-bsp/sources/poky/meta/recipes-devtools/apt/apt_2.4.5.bb:do_populate_sysroot', 'virtual:native:/home/arash/Desktop/imx-yocto-bsp/sources/poky/meta/recipes-devtools/dosfstools/dosfstools_4.2.bb:do_populate_sysroot', 'virtual:native:/home/arash/Desktop/imx-yocto-bsp/sources/poky/meta/recipes-devtools/dpkg/dpkg_1.21.4.bb:do_populate_sysroot', 'virtual:native:/home/arash/Desktop/imx-yocto-bsp/sources/poky/meta/recipes-devtools/e2fsprogs/e2fsprogs_1.46.5.bb:do_populate_sysroot', 'virtual:native:/home/arash/Desktop/imx-yocto-bsp/sources/poky/meta/recipes-devtools/fdisk/gptfdisk_1.0.8.bb:do_populate_sysroot', 'virtual:native:/home/arash/Desktop/imx-yocto-bsp/sources/poky/meta/recipes-devtools/makedevs/makedevs_1.0.1.bb:do_populate_sysroot', 'virtual:native:/home/arash/Desktop/imx-yocto-bsp/sources/poky/meta/recipes-devtools/mtools/mtools_4.0.38.bb:do_populate_sysroot', 'virtual:native:/home/arash/Desktop/imx-yocto-bsp/sources/poky/meta/recipes-devtools/opkg-utils/opkg-utils_0.5.0.bb:do_populate_sysroot', 'virtual:native:/home/arash/Desktop/imx-yocto-bsp/sources/poky/meta/recipes-devtools/pseudo/pseudo_git.bb:do_populate_sysroot', 'virtual:native:/home/arash/Desktop/imx-yocto-bsp/sources/poky/meta/recipes-extended/parted/parted_3.4.bb:do_populate_sysroot', 'virtual:native:/home/arash/Desktop/imx-yocto-bsp/sources/poky/meta/recipes-extended/pigz/pigz_2.7.bb:do_populate_sysroot', 'virtual:native:/home/arash/Desktop/imx-yocto-bsp/sources/poky/meta/recipes-extended/zstd/zstd_1.5.2.bb:do_populate_sysroot', 'virtual:native:/home/arash/Desktop/imx-yocto-bsp/sources/poky/meta/recipes-support/bmap-tools/bmap-tools_git.bb:do_populate_sysroot']
| NOTE: Installed into sysroot: []
| NOTE: Skipping as already exists in sysroot: ['imx-boot', 'u-boot-imx', 'imx-m7-demos', 'cross-localedef-native', 'ldconfig-native', 'qemuwrapper-cross', 'depmodwrapper-cross', 'update-rc.d-native', 'apt-native', 'dosfstools-native', 'dpkg-native', 'e2fsprogs-native', 'gptfdisk-native', 'makedevs-native', 'mtools-native', 'opkg-utils-native', 'pseudo-native', 'parted-native', 'pigz-native', 'zstd-native', 'bmap-tools-native', 'qemu-native', 'desktop-file-utils-native', 'gdk-pixbuf-native', 'systemd-systemctl-native', 'gtk+3-native', 'shadow-native', 'optee-os', 'firmware-imx-8m', 'gcc-runtime', 'imx-atf', 'glibc', 'nss-native', 'kmod-native', 'perl-native', 'libtool-native', 'readline-native', 'xz-native', 'util-linux-native', 'texinfo-dummy-native', 'gettext-minimal-native', 'ncurses-native', 'lz4-native', 'zlib-native', 'libgcrypt-native', 'cmake-native', 'gnutls-native', 'xxhash-native', 'db-native', 'glib-2.0-native', 'popt-native', 'python3-installer-native', 'python3-wheel-native', 'python3-six-native', 'python3-setuptools-native', 'python3-native', 'coreutils-native', 'debianutils-native', 'openssl-native', 'bzip2-native', 'gettext-native', 'attr-native', 'shared-mime-info-native', 'libjpeg-turbo-native', 'libpng-native', 'gobject-introspection-native', 'libx11-native', 'atk-native', 'libxrandr-native', 'pango-native', 'cairo-native', 'libxcomposite-native', 'at-spi2-atk-native', 'fontconfig-native', 'libxext-native', 'libxcursor-native', 'libxfixes-native', 'libxrender-native', 'libxdamage-native', 'libxi-native', 'libgcc', 'linux-libc-headers', 'sqlite3-native', 'nspr-native', 'gdbm-native', 'make-native', 'util-linux-libuuid-native', 'libcap-ng-native', 'libpcre2-native', 'libgpg-error-native', 'libcap-native', 'curl-native', 'libunistring-native', 'p11-kit-native', 'nettle-native', 'gmp-native', 'libidn2-native', 'libffi-native', 'libpcre-native', 'python3-flit-core-native', 'unzip-native', 'libnsl2-native', 'libtirpc-native', 'libxml2-native', 'itstool-native', 'flex-native', 'xorgproto-native', 'libxcb-native', 'util-macros-native', 'xtrans-native', 'fribidi-native', 'freetype-native', 'harfbuzz-native', 'libxft-native', 'pixman-native', 'libsm-native', 'dbus-native', 'at-spi2-core-native', 'expat-native', 'libtasn1-native', 'm4-native', 'libxau-native', 'libxdmcp-native', 'xcb-proto-native', 'libpthread-stubs-native', 'icu-native', 'libice-native', 'libxtst-native', 'gnu-config-native']
| DEBUG: Python function extend_recipe_sysroot finished
| DEBUG: Executing python function set_image_size
| DEBUG: 6201384.800000 = 4770296 * 1.300000
| DEBUG: 56201384.800000 = max(6201384.800000, 65536)[6201384.800000] + 50000000
| DEBUG: 56201385.000000 = int(56201384.800000)
| DEBUG: 56201385 = aligned(56201385)
| DEBUG: returning 56201385
| DEBUG: Python function set_image_size finished
| DEBUG: Executing shell function do_image_wic
| INFO: Creating image(s)...
|
| Traceback (most recent call last):
| File "/home/arash/Desktop/imx-yocto-bsp/sources/poky/scripts/lib/wic/filemap.py", line 129, in _open_image_file
| self._f_image = open(self._image_path, 'rb')
| FileNotFoundError: [Errno 2] No such file or directory: '/home/arash/Desktop/imx-yocto-bsp/build-wayland/tmp/deploy/images/imx8mp-lpddr4-evk/imx-boot'
|
| During handling of the above exception, another exception occurred:
|
| Traceback (most recent call last):
| File "/home/arash/Desktop/imx-yocto-bsp/sources/poky/scripts/wic", line 547, in <module>
| sys.exit(main(sys.argv[1:]))
| File "/home/arash/Desktop/imx-yocto-bsp/sources/poky/scripts/wic", line 542, in main
| return hlp.invoke_subcommand(args, parser, hlp.wic_help_usage, subcommands)
| File "/home/arash/Desktop/imx-yocto-bsp/sources/poky/scripts/lib/wic/help.py", line 83, in invoke_subcommand
| subcmd[0](args, usage)
| File "/home/arash/Desktop/imx-yocto-bsp/sources/poky/scripts/wic", line 222, in wic_create_subcommand
| engine.wic_create(wks_file, rootfs_dir, bootimg_dir, kernel_dir,
| File "/home/arash/Desktop/imx-yocto-bsp/sources/poky/scripts/lib/wic/engine.py", line 190, in wic_create
| plugin.do_create()
| File "/home/arash/Desktop/imx-yocto-bsp/sources/poky/scripts/lib/wic/plugins/imager/direct.py", line 98, in do_create
| self.create()
| File "/home/arash/Desktop/imx-yocto-bsp/sources/poky/scripts/lib/wic/plugins/imager/direct.py", line 182, in create
| self._image.prepare(self)
| File "/home/arash/Desktop/imx-yocto-bsp/sources/poky/scripts/lib/wic/plugins/imager/direct.py", line 360, in prepare
| part.prepare(imager, imager.workdir, imager.oe_builddir,
| File "/home/arash/Desktop/imx-yocto-bsp/sources/poky/scripts/lib/wic/partition.py", line 183, in prepare
| plugin.do_prepare_partition(self, srcparams_dict, creator,
| File "/home/arash/Desktop/imx-yocto-bsp/sources/poky/scripts/lib/wic/plugins/source/rawcopy.py", line 95, in do_prepare_partition
| sparse_copy(src, dst)
| File "/home/arash/Desktop/imx-yocto-bsp/sources/poky/scripts/lib/wic/filemap.py", line 527, in sparse_copy
| fmap = api(src_fname)
| File "/home/arash/Desktop/imx-yocto-bsp/sources/poky/scripts/lib/wic/filemap.py", line 506, in filemap
| return FilemapFiemap(image, log)
| File "/home/arash/Desktop/imx-yocto-bsp/sources/poky/scripts/lib/wic/filemap.py", line 323, in __init__
| _FilemapBase.__init__(self, image, log)
| File "/home/arash/Desktop/imx-yocto-bsp/sources/poky/scripts/lib/wic/filemap.py", line 88, in __init__
| self._open_image_file()
| File "/home/arash/Desktop/imx-yocto-bsp/sources/poky/scripts/lib/wic/filemap.py", line 131, in _open_image_file
| raise Error("cannot open image file '%s': %s"
| wic.filemap.Error: cannot open image file '/home/arash/Desktop/imx-yocto-bsp/build-wayland/tmp/deploy/images/imx8mp-lpddr4-evk/imx-boot': [Errno 2] No such file or directory: '/home/arash/Desktop/imx-yocto-bsp/build-wayland/tmp/deploy/images/imx8mp-lpddr4-evk/imx-boot'
| WARNING: exit code 1 from a shell command.
ERROR: Task (/home/arash/Desktop/imx-yocto-bsp/sources/meta-imx/meta-sdk/dynamic-layers/qt6-layer/recipes-fsl/images/imx-image-full.bb:do_image_wic) failed with exit code '1'
NOTE: Tasks Summary: Attempted 9991 tasks of which 9990 didn't need to be rerun and 1 failed.

Summary: 1 task failed:
/home/arash/Desktop/imx-yocto-bsp/sources/meta-imx/meta-sdk/dynamic-layers/qt6-layer/recipes-fsl/images/imx-image-full.bb:do_image_wic
Summary: There was 1 WARNING message.
Summary: There was 1 ERROR message, returning a non-zero exit code.


could you help me for correct this error. thanks alot.

0 项奖励
回复
4 回复数

2,486 次查看
jimmychan
NXP TechSupport
NXP TechSupport

Which version of BSP are you using?

 

0 项奖励
回复

2,473 次查看
arash_eng
Contributor I

hi jimmychan,

I'm using L5.15.71_2.2.0 BSP linux.

0 项奖励
回复

2,401 次查看
jimmychan
NXP TechSupport
NXP TechSupport

Hello,

 

Please check the minimum Ubuntu version is required 20.04 or later.

And please check the following host packages are updated.

$ sudo apt-get install gawk wget git-core diffstat unzip texinfo gcc-multilib
build-essential chrpath socat cpio python python3 python3-pip python3-pexpect
xz-utils debianutils iputils-ping python3-git python3-jinja2 libegl1-mesa libsdl1.2-dev
pylint3 xterm rsync curl zstd pzstd lz4c lz4 libssl-dev

0 项奖励
回复

2,366 次查看
arash_eng
Contributor I

hello again,

 

my host ubuntu version is 22.04.2, and the libraries were updated.

some of the libraries are not unable for my ubuntu like pylint3 pzstd lz4c but I don't think the problem accrued for them. if you have more details, I will be grateful for more explanation.

 

 

 

0 项奖励
回复