imx 7dual eMMc bitbake error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx 7dual eMMc bitbake error

3,352 次查看
nhpark
Contributor II

2022-10-04 10;41;13.PNG

2022-10-04 10;41;48.png

   

I want to create emmc bootloader with bitbake. But I get an error during bitbake. Attach a picture of the environment configuration and error message capture. I want to know which manual I should refer to and why the error occurs.

标记 (2)
0 项奖励
回复
5 回复数

3,299 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Hi 

The "DISTRO" should be fsl-imx-xwayland not fsl-xwayland. You can change it from the "local.conf" that you posted

I'd recommend you build from scratch with the correct DISTRO, the distro name will be fsl-imx-xwayland

DISTRO=<distro name> MACHINE=<machine name> source imx-setup-release.sh -b <build dir>

Regarding "create emmc bootloader with bitbake" 

With successful completion of yocto build, you will see all files under the directory: <your build directory>/tmp/deploy/images/

You can refer to github.com for how to burn bootloader to eMMC to start.

 

Best regards

Harvey

 

0 项奖励
回复

3,297 次查看
nhpark
Contributor II

The files were successfully created when bitbake core-image-minimal was executed except for UBOOT_CONFIG = "emmc" in local.conf. But when I add UBOOT_CONFIG = "emmc", it keeps failing. This time I ran bitbake core-image-minimal with fsl-imx-xwayland with DISTRO, but it still failed. I'll attach a picture of the configuration and error message. I need initramfs, dtb, zimage, rootfs, bootloader for burning to emmc. The helpful link has instructions on how to use uuu, but no instructions on bitbake to create the files used for uuu. I first create the files I mentioned above with bitbake.

2022-10-21 09;10;50.PNG

2022-10-21 09;12;00.PNG

  

0 项奖励
回复

3,336 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Hi @nhpark 

The DISTRO fsl-imx-x11 is not supported anymore. 

Harvey021_1-1665288657880.png

 

Best regards

Harvey

0 项奖励
回复

3,271 次查看
nhpark
Contributor II

....?????????????

0 项奖励
回复

3,311 次查看
nhpark
Contributor II

Thanks for the support. I changed the setting to xwayland, but the error still occurs.

I don't know how to change the configuration. I refer to these documents, IMX_LINUX_USERS_GUIDE, IMX_PORTING_GUIDE, IMX_YOCTO_PROJECT_USERS_GUIDE, but I do not know the process for bitbake with EMMC. Is there any documentation I should refer to further? I would like to know the configuration and bitbake command for bitbake with emmc.

2022-10-19 09;18;02.PNG

2022-10-19 09;22;03.PNG

 

0 项奖励
回复