imx 6 sdio 3.0 enable support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx 6 sdio 3.0 enable support

2,445件の閲覧回数
keithchang
Contributor I

Dear,

After reading below discussion in Freescale community, Freescale people mentioned someone enabled SDIO 3.0 and we can contact local team for the issue. Could you help to share with us in the information about enabling SDIO 3.0 (customer/third party etc.)? Appreciated your help.

imx 6 sdio 3.0

BR

Keith

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,829件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Keith

you can check attached files and link below

linux-2.6-imx.git - Freescale i.MX Linux Tree

Customer info is private and can not be shared, sorry.

Best regards

igor

0 件の賞賛
返信

1,829件の閲覧回数
keithchang
Contributor I

Dear Igor,

Appreciated your help and information. Could you help to provide the information of following questions in advance? Thanks.

1) Did the test use real AP to get the throughput? If yes, could you provide the type/name of the real AP? We will reproduce the environment in our side.

2) Did the test use 2x2 MIMO in this throughput test?

3) Since BCM43241 supports 802.11 a/b/g/n, HS mode should be enough for support 802.11n, is it?

4) Do the patches of 'sabre ai sdio 3.0_patches.zip' be used to verify 802.11ac before?

Best regards

Keith

0 件の賞賛
返信