imx 6 platform using gstreamer to displaye 4 camears,when quit, the kernel panic

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx 6 platform using gstreamer to displaye 4 camears,when quit, the kernel panic

992 次查看
xiaoqiya
Contributor I

My Command as follow:

gst-launch v4l2src device=/dev/video0  ! 'video/x-raw-yuv, format=(fourcc)UYVY' ! queue ! mfw_isink disp-width=512 d

gst-launch v4l2src device=/dev/video1  ! 'video/x-raw-yuv, format=(fourcc)UYVY' ! queue ! mfw_isink disp-width=512 d

gst-launch v4l2src device=/dev/video2  ! 'video/x-raw-yuv, format=(fourcc)UYVY' ! queue ! mfw_isink disp-width=512 d

gst-launch v4l2src device=/dev/video3  ! 'video/x-raw-yuv, format=(fourcc)UYVY' ! queue ! mfw_isink disp-width=512 d

when i want to shutdown the camera, i use "kill -2 pid1 pid2 pid3 pid4" ,but the system damaged and the following error appears:

ExecuUnable to handle kernel paging request at virtual address ca499000

tion ended after 1000159667 ns.

pgd = b8524000

Setting pipeline to PAUSED ...

h[ca499000] *pgd=4886e811andling interrupt.

Interrupt: St, *pte=00000000opping pipeline ...

Execution en, *ppte=00000000ded after 1000581001 ns.

Setting

pipeline to PAUSED ...

Setting Internal error: Oops: 807 [#1] PREEMPT SMP

Modules linked in:

CPU: 0    Not tainted  (3.0.35 #2)

PC is at memcpy+0x50/0x330

LR is at 0x407040c0

pc : [<802355b0>]    lr : [<407040c0>]    psr: 20000113

sp : b80a7d54  ip : 407040c0  fp : 80afda70

r10: 00000b40  r9 : 8003d278  r8 : 407040c0

r7 : 407040c0  r6 : 407040c0  r5 : 407040c0  r4 : 407040c0

r3 : 407040c0  r2 : 00000180  r1 : ff9949e0  r0 : ca499000

Flags: nzCv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment user

Control: 10c53c7d  Table: 4852404a  DAC: 00000015

Process gst-launch-0.10 (pid: 3401, stack limit = 0xb80a62f0)

Stack: (0xb80a7d54 to 0xb80a8000)

The probability of the error is more than 50%(other 50%   4 cameras quit normal).

Is there any other methods to quit gstreamer or is there bug in the official plugins of v4l2src or mfw_isink?

who can help me ...thanks

标签 (1)
0 项奖励
回复
1 回复

841 次查看
igorpadykov
NXP Employee
NXP Employee

Hi XiaoQi

please check below how to crrectly stop pipeline

reg: gst-launch stop command

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复