imx 535 sata bug

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx 535 sata bug

1,995 Views
lengyu
Contributor I

Hi,

I view the websitsQ&A:How to mount SATA disk for rootfs?

Now, we have many devices which use imx535, concentrated bursts this problems.

log:

...

ata1: SATA max UDMA/133 irq_stat 0x00000040, connection status changed irq 28

...

ata1: SATA link down (SStatus 1 SControl 300)

ata1: exception Emask 0x10 SAct 0x0 SErr 0x4000000 action 0xe frozen t4

ata1: irq_stat 0x00000040, connection status changed

ata1: SError: { DevExch }

ata1: hard resetting link

ata1: SATA link down (SStatus 1 SControl 300)

ata1: EH complete

"""

Now, we want one solution for this bug. On the websits we know linux 3.2 version this bug was fixed, So where can we get this version?

TKS.

0 Kudos
Reply
1 Reply

1,710 Views
igorpadykov
NXP Employee
NXP Employee

Hi li

I think most latest thoroughly tested i.MX53 images are on link below

Public images - fsl-community-bsp/master/389/framebuffer/imx53qsb

Please post this to meta-fsl-arm mailing list, so that someone familiar with

latest kernels could try to assist you.

https://lists.yoctoproject.org/listinfo/meta-freescale

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply