imx 535 sata bug

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx 535 sata bug

1,981件の閲覧回数
lengyu
Contributor I

Hi,

I view the websitsQ&A:How to mount SATA disk for rootfs?

Now, we have many devices which use imx535, concentrated bursts this problems.

log:

...

ata1: SATA max UDMA/133 irq_stat 0x00000040, connection status changed irq 28

...

ata1: SATA link down (SStatus 1 SControl 300)

ata1: exception Emask 0x10 SAct 0x0 SErr 0x4000000 action 0xe frozen t4

ata1: irq_stat 0x00000040, connection status changed

ata1: SError: { DevExch }

ata1: hard resetting link

ata1: SATA link down (SStatus 1 SControl 300)

ata1: EH complete

"""

Now, we want one solution for this bug. On the websits we know linux 3.2 version this bug was fixed, So where can we get this version?

TKS.

ラベル(7)
0 件の賞賛
返信
1 返信

1,696件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi li

I think most latest thoroughly tested i.MX53 images are on link below

Public images - fsl-community-bsp/master/389/framebuffer/imx53qsb

Please post this to meta-fsl-arm mailing list, so that someone familiar with

latest kernels could try to assist you.

https://lists.yoctoproject.org/listinfo/meta-freescale

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信