imx-4.19.35-1.1.0.xml updated to incorrect SHA for https://source.codeaurora.org/external/imx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx-4.19.35-1.1.0.xml updated to incorrect SHA for https://source.codeaurora.org/external/imx

1,098件の閲覧回数
vincentz63
Contributor IV

File imx-4.19.35-1.1.0.xml in repo https://source.codeaurora.org/external/imx/imx-manifest was updated to pull the wrong revision for the CAF repo:

- <project remote="CAF" revision="6b237a975521daa1687c5ac49f57da6d32c8c719" name="meta-fsl-bsp-release" path="sources/meta-fsl-bsp-release" upstream="warrior-4.19.35-1.1.0" >
+ <project remote="CAF" revision="b2c6e41596b8d068232e0a5fddf2675aa57ec92a" name="meta-fsl-bsp-release" path="sources/meta-fsl-bsp-release" upstream="warrior-4.19.35-1.1.0" >

The update was done in commit 0d1e92b4b7d432fb9456fc9fcdf3586114c6fbda by Tom Hochstein <[email protected]> on Wed Apr 6 16:24:27 2022 -0500.

The next commit replaces the SHA with a tag name, and is also invalid.

I believe this is a mistake as this commits changes the source code used for an existing release, which should never happen, and breaks the build in the process! (It no longer overwrites the meta-freescale machine conf files.)

タグ(2)
0 件の賞賛
返信
0 返答(返信)