yocto5.15 spi-slave

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

yocto5.15 spi-slave

683 Views
lljwork2021
Contributor I

root@imx8qxpc0mek:/sys/class/spi_slave/spi3# ls
device of_node power slave spi3.0 statistics subsystem uevent

spi3.0 cannot be generated in the /dev directory.

In versions 4.14 and 5.4, it is possible to build SPI devices in the /dev directory. Version 5.15 fails.

I suspect there is a problem with the IMX driver or a new SPI driver framework.

 

 

0 Kudos
Reply
0 Replies