implement the digital zoom function of camera

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

implement the digital zoom function of camera

1,502 Views
ninglu
Contributor II
We are using imx6-sabresd board ,and system is android 4.4.2.Using ov5640 camera.

     We want to implement the digital zoom function of camera.

who can tell me how to do?

Tags (1)
0 Kudos
Reply
3 Replies

1,112 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Digital zoom may be performed as image resizing (with interpolation)
via IPU on i.MX6. For more details please refer to IPU driver description in
“i.MX_Linux_Reference_Manual.pdf” and IPU chapter in the i.MX6 Reference
Manual.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,112 Views
ninglu
Contributor II

I have read this manual, but I still don't know how to achieve digital zoom in the code。

Could you give me an example

0 Kudos
Reply

1,112 Views
Yuri
NXP Employee
NXP Employee

Hello

The following may be useful :


rogeriorps/ipu-examples · GitHub

Also You may look at section 6.4.3 (IPU Device Unit test) of

“i.MX_6_Linux_Reference_Manual.pdf”.

http://www.nxp.com/webapp/Download?colCode=L3.14.52_1.1.0_LINUX_DOC

Regards,

Yuri.

0 Kudos
Reply