implement the digital zoom function of camera

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

implement the digital zoom function of camera

1,535件の閲覧回数
ninglu
Contributor II
We are using imx6-sabresd board ,and system is android 4.4.2.Using ov5640 camera.

     We want to implement the digital zoom function of camera.

who can tell me how to do?

ラベル(5)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

1,145件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Digital zoom may be performed as image resizing (with interpolation)
via IPU on i.MX6. For more details please refer to IPU driver description in
“i.MX_Linux_Reference_Manual.pdf” and IPU chapter in the i.MX6 Reference
Manual.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,145件の閲覧回数
ninglu
Contributor II

I have read this manual, but I still don't know how to achieve digital zoom in the code。

Could you give me an example

0 件の賞賛
返信

1,145件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello

The following may be useful :


rogeriorps/ipu-examples · GitHub

Also You may look at section 6.4.3 (IPU Device Unit test) of

“i.MX_6_Linux_Reference_Manual.pdf”.

http://www.nxp.com/webapp/Download?colCode=L3.14.52_1.1.0_LINUX_DOC

Regards,

Yuri.

0 件の賞賛
返信