im6sl android init failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

im6sl android init failed

3,114件の閲覧回数
zhghua1103
Contributor I

Dear ALL,

Thanks very much for your help about the important  question,

such as:

boota mmc0                                                                      
kernel   @ 82808000 (8723568)                                                   
ramdisk  @ 83800000 (1027620)                                                   
fdt      @ 83700000 (36758)                                                     
## Booting Android Image at 0x80800000 ...                                      
Kernel load addr 0x82808000 size 8520 KiB                                       
Kernel command line: console=ttymxc0,115200 init=/init androidboot.console=ttyme
## Flattened Device Tree blob at 83700000                                       
   Booting using the fdt blob at 0x83700000                                     
   Loading Kernel Image ... OK                                                  
   Using Device Tree in place at 83700000, end 8370bf95                         
switch to ldo_bypass mode!                                                      
                                                                                
Starting kernel ...                                                             
                                                                                
Booting Linux on physical CPU 0x0                                               
Initializing cgroup subsys cpu                                                  
Initializing cgroup subsys cpuacct                                              
Linux version 4.1.15-dirty (root@joshua) (gcc version 4.9.x-google 20140827 (pr6
CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d                
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache        
Machine model: Freescale i.MX6 SoloLite EVK Board                               
Reserved memory: created CMA memory pool at 0x9a000000, size 320 MiB            
Reserved memory: initialized node linux,cma, compatible id shared-dma-pool      
Memory policy: Data cache writealloc                                            
PERCPU: Embedded 13 pages/cpu @eef2d000 s22144 r8192 d22912 u53248              
Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 260368     
Kernel command line: console=ttymxc0,115200 init=/init androidboot.console=ttymd
PID hash table entries: 4096 (order: 2, 16384 bytes)                            
Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)                
Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)                  
Memory: 690984K/1047552K available (11566K kernel code, 972K rwdata, 3688K roda)
Virtual kernel memory layout:                                                   
    vector  : 0xffff0000 - 0xffff1000   (   4 kB)                               
    fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)                               
    vmalloc : 0xf0000000 - 0xff000000   ( 240 MB)                               
    lowmem  : 0xc0000000 - 0xef800000   ( 760 MB)                               
    pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)                               
    modules : 0xbf000000 - 0xbfe00000   (  14 MB)                               
      .text : 0xc0008000 - 0xc0fe5a34   (16247 kB)                              
      .init : 0xc1000000 - 0xc1100000   (1024 kB)                               
      .data : 0xc1100000 - 0xc11f33d0   ( 973 kB)                               
       .bss : 0xc11f33d0 - 0xc1296f64   ( 655 kB)                               
SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1                      
Preemptible hierarchical RCU implementation.                                    
        Additional per-CPU info printed with stalls.                            
        RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=1.                    
RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1                    
NR_IRQS:16 nr_irqs:16 16                                                        
L2C-310 erratum 769419 enabled                                                  
L2C-310 enabling early BRESP for Cortex-A9                                      
L2C-310 full line of zeros enabled for Cortex-A9                                
L2C-310 ID prefetch enabled, offset 16 lines                                    
L2C-310 dynamic clock gating enabled, standby mode enabled                      
L2C-310 cache controller enabled, 16 ways, 256 kB                               
L2C-310: CACHE_ID 0x410000c8, AUX_CTRL 0x76030001                               
mxc_clocksource_init 24000000                                                   
Switching to timer-based delay loop, resolution 41ns                            
sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns       
clocksource mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7s
Console: colour dummy device 80x30                                              
Calibrating delay loop (skipped), value calculated using timer frequency.. 48.0)
pid_max: default: 32768 minimum: 301                                            
Security Framework initialized                                                  
SELinux:  Initializing.                                                         
AppArmor: AppArmor disabled by boot time parameter                              
Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)                     
Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)                
Initializing cgroup subsys freezer                                              
Initializing cgroup subsys debug                                                
CPU: Testing write buffer coherency: ok                                         
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000                                
Setting up static identity map for 0x80100000 - 0x80100058                      
Brought up 1 CPUs                                                               
SMP: Total of 1 processors activated (48.00 BogoMIPS).                          
CPU: All CPU(s) started in SVC mode.                                            
devtmpfs: initialized                                                           
device-tree: Duplicate name in lcdif@020f8000, renamed to "display#1"           
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4         
clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 1911s
pinctrl core: initialized pinctrl subsystem                                     
NET: Registered protocol family 16                                              
DMA: preallocated 256 KiB pool for atomic coherent allocations                  
cpuidle: using governor ladder                                                  
cpuidle: using governor menu                                                    
anatop_regulator 20c8000.anatop:regulator-vddcore@140: Failed to read a valid d.
anatop_regulator: probe of 20c8000.anatop:regulator-vddcore@140 failed with err2
anatop_regulator 20c8000.anatop:regulator-vddsoc@140: Failed to read a valid de.
anatop_regulator: probe of 20c8000.anatop:regulator-vddsoc@140 failed with erro2
hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.     
hw-breakpoint: maximum watchpoint size is 4 bytes.                              
VDSO is not a valid ELF object!                                                 
imx6sl-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver                   
SCSI subsystem initialized                                                      
usbcore: registered new interface driver usbfs                                  
usbcore: registered new interface driver hub                                    
usbcore: registered new device driver usb                                       
2000000.aips-bus:usbphy_nop1 supply vcc not found, using dummy regulator        
0-0048 supply SENSOR not found, using dummy regulator                           
i2c i2c-0: Max17135 PMIC not found!                                             
i2c i2c-0: IMX I2C adapter registered                                           
i2c i2c-0: can't use DMA                                                        
i2c i2c-1: IMX I2C adapter registered                                           
i2c i2c-1: can't use DMA                                                        
i2c i2c-2: IMX I2C adapter registered                                           
i2c i2c-2: can't use DMA                                                        
Linux video capture interface: v2.00                                            
pps_core: LinuxPPS API ver. 1 registered                                        
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@>
PTP clock support registered                                                    
MIPI CSI2 driver module loaded                                                  
Advanced Linux Sound Architecture Driver Initialized.                           
Bluetooth: Core ver 2.20                                                        
NET: Registered protocol family 31                                              
Bluetooth: HCI device and connection manager initialized                        
Bluetooth: HCI socket layer initialized                                         
Bluetooth: L2CAP socket layer initialized                                       
Bluetooth: SCO socket layer initialized                                         
Switched to clocksource mxc_timer1                                              
NET: Registered protocol family 2                                               
TCP established hash table entries: 8192 (order: 3, 32768 bytes)                
TCP bind hash table entries: 8192 (order: 4, 65536 bytes)                       
TCP: Hash tables configured (established 8192 bind 8192)                        
UDP hash table entries: 512 (order: 2, 16384 bytes)                             
UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)                        
NET: Registered protocol family 1                                               
RPC: Registered named UNIX socket transport module.                             
RPC: Registered udp transport module.                                           
RPC: Registered tcp transport module.                                           
RPC: Registered tcp NFSv4.1 backchannel transport module.                       
Trying to unpack rootfs image as initramfs...                                   
Freeing initrd memory: 1004K (c3800000 - c38fb000)                              
CPU PMU: Failed to parse /soc/pmu/interrupt-affinity[0]                         
hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available    
imx rpmsg driver is registered.                                                 
Bus freq driver module loaded                                                   
console [pstore-1] enabled                                                      
pstore: Registered ramoops as persistent store backend                          
ramoops: attached 0x100000@0xbbf00000, ecc: 0/0                                 
mxc_ramoops device success loaded                                               
futex hash table entries: 256 (order: 2, 16384 bytes)                           
audit: initializing netlink subsys (disabled)                                   
audit: type=2000 audit(0.360:1): initialized                                    
VFS: Disk quotas dquot_6.6.0                                                    
VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)                 
NFS: Registering the id_resolver key type                                       
Key type id_resolver registered                                                 
Key type id_legacy registered                                                   
ntfs: driver 2.1.32 [Flags: R/W DEBUG].                                         
jffs2: version 2.2. (NAND) �© 2001-2006 Red Hat, Inc.                           
fuse init (API version 7.23)                                                    
bounce: pool size: 64 pages                                                     
io scheduler noop registered                                                    
io scheduler deadline registered                                                
io scheduler cfq registered (default)                                           
pwm-backlight supply power not found, using dummy regulator                     
MIPI DSI driver module loaded                                                   
MIPI DSI driver module loaded                                                   
sii902x 1-0039: Sii902x: cound not find device                                  
mxsfb 20f8000.lcdif: failed to find mxc display driver                          
Console: switching to colour frame buffer device 100x30                         
mxsfb 20f8000.lcdif: initialized                                                
imx-sdma 20ec000.sdma: no event needs to be remapped                            
imx-sdma 20ec000.sdma: loaded firmware 3.3                                      
imx-sdma 20ec000.sdma: initialized                                              
pfuze100-regulator 0-0008: Full layer: 2, Metal layer: 1                        
pfuze100-regulator 0-0008: FAB: 0, FIN: 0                                       
pfuze100-regulator 0-0008: pfuze100 found.                                      
2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 21, base_baud = 5000000) is a X
console [ttymxc0] enabled                                                       
imx sema4 driver is registered.                                                 
[drm] Initialized drm 1.1.0 20060810                                            
[drm] Initialized vivante 1.0.0 20120216 on minor 0                             
brd: module loaded                                                              
loop: module loaded                                                             
zram: Created 1 device(s)                                                       
m25p80 spi0.0: unrecognized JEDEC id bytes: 00,  0,  0                          
spi_imx 2008000.ecspi: probed                                                   
tun: Universal TUN/TAP device driver, 1.6                                       
tun: (C) 1999-2004 Max Krasnyansky <[email protected]>                          
CAN device driver interface                                                     
2188000.ethernet supply phy not found, using dummy regulator                    
libphy: fec_enet_mii_bus: probed                                                
PPP generic driver version 2.4.2                                                
PPP BSD Compression module registered                                           
PPP Deflate Compression module registered                                       
PPP MPPE Compression module registered                                          
NET: Registered protocol family 24                                              
pegasus: v0.9.3 (2013/04/25), Pegasus/Pegasus II USB Ethernet driver            
usbcore: registered new interface driver pegasus                                
usbcore: registered new interface driver rtl8150                                
usbcore: registered new interface driver r8152                                  
usbcore: registered new interface driver asix                                   
usbcore: registered new interface driver ax88179_178a                           
usbcore: registered new interface driver cdc_ether                              
usbcore: registered new interface driver cdc_eem                                
usbcore: registered new interface driver net1080                                
usbcore: registered new interface driver cdc_subset                             
usbcore: registered new interface driver zaurus                                 
usbcore: registered new interface driver cdc_ncm                                
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver                      
ehci-mxc: Freescale On-Chip EHCI Host driver                                    
usbcore: registered new interface driver cdc_acm                                
cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters     
usbcore: registered new interface driver usb-storage                            
usbcore: registered new interface driver usbserial                              
usbcore: registered new interface driver usbserial_generic                      
usbserial: USB Serial support registered for generic                            
usbcore: registered new interface driver ftdi_sio                               
usbserial: USB Serial support registered for FTDI USB Serial Device             
usbcore: registered new interface driver option                                 
usbserial: USB Serial support registered for GSM modem (1-port)                 
usbcore: registered new interface driver usb_ehset_test                         
usb_otg1_vbus: supplied by SWBST                                                
usb_otg2_vbus: supplied by SWBST                                                
ci_hdrc ci_hdrc.1: EHCI Host Controller                                         
ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1                
ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00                                   
usb usb1: New USB device found, idVendor=1d6b, idProduct=0002                   
usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1              
usb usb1: Product: EHCI Host Controller                                         
usb usb1: Manufacturer: Linux 4.1.15-dirty ehci_hcd                             
usb usb1: SerialNumber: ci_hdrc.1                                               
hub 1-0:1.0: USB hub found                                                      
hub 1-0:1.0: 1 port detected                                                    
mousedev: PS/2 mouse device common for all mice                                 
input: 20b8000.kpp as /devices/soc0/soc/2000000.aips-bus/20b8000.kpp/input/inpu0
usbcore: registered new interface driver xpad                                   
usbcore: registered new interface driver usb_acecad                             
usbcore: registered new interface driver aiptek                                 
usbcore: registered new interface driver gtco                                   
usbcore: registered new interface driver hanwang                                
usbcore: registered new interface driver kbtab                                  
mma8450 0-001c: read chip ID 0xfffffffb is not equal to 0xc6!                   
mma8450: probe of 0-001c failed with error -22                                  
snvs_rtc 20cc000.snvs:snvs-rtc-lp: rtc core: registered 20cc000.snvs:snvs-r as 0
i2c /dev entries driver                                                         
IR NEC protocol handler initialized                                             
IR RC5(x/sz) protocol handler initialized                                       
IR RC6 protocol handler initialized                                             
IR JVC protocol handler initialized                                             
IR Sony protocol handler initialized                                            
IR SANYO protocol handler initialized                                           
IR Sharp protocol handler initialized                                           
IR MCE Keyboard/mouse protocol handler initialized                              
IR XMP protocol handler initialized                                             
2-003c supply DOVDD not found, using dummy regulator                            
ov5640_read_reg:write reg error:reg=300a                                        
camera ov5640 is not found                                                      
pxp-v4l2 pxp_v4l2_out: initialized                                              
usbcore: registered new interface driver uvcvideo                               
USB Video Class driver (1.1.1)                                                  
imx2-wdt 20bc000.wdog: timeout 60 sec (nowayout=0)                              
device-mapper: uevent: version 1.0.3                                            
device-mapper: ioctl: 4.31.0-ioctl (2015-3-12) initialised: [email protected]
Bluetooth: HCI UART driver ver 2.3                                              
Bluetooth: HCI UART protocol H4 registered                                      
Bluetooth: HCI UART protocol BCSP registered                                    
Bluetooth: HCI UART protocol ATH3K registered                                   
usbcore: registered new interface driver btusb                                  
sdhci: Secure Digital Host Controller Interface driver                          
sdhci: Copyright(c) Pierre Ossman                                               
sdhci-pltfm: SDHCI platform and OF driver helper                                
/soc/aips-bus@02100000/usdhc@02190000: voltage-ranges unspecified               
sdhci-esdhc-imx 2190000.usdhc: could not get ultra high speed state, work on noe
sdhci-esdhc-imx 2190000.usdhc: Got WP GPIO                                      
sdhci-esdhc-imx 2190000.usdhc: assigned as wifi host                            
sdhci-esdhc-imx 2190000.usdhc: No vmmc regulator found                          
sdhci-esdhc-imx 2190000.usdhc: No vqmmc regulator found                         
mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using DMA               
/soc/aips-bus@02100000/usdhc@02194000: voltage-ranges unspecified               
sdhci-esdhc-imx 2194000.usdhc: Got CD GPIO                                      
sdhci-esdhc-imx 2194000.usdhc: Got WP GPIO                                      
sdhci-esdhc-imx 2194000.usdhc: No vmmc regulator found                          
sdhci-esdhc-imx 2194000.usdhc: No vqmmc regulator found                         
mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using DMA               
/soc/aips-bus@02100000/usdhc@02198000: voltage-ranges unspecified               
sdhci-esdhc-imx 2198000.usdhc: could not get ultra high speed state, work on noe
sdhci-esdhc-imx 2198000.usdhc: No vmmc regulator found                          
sdhci-esdhc-imx 2198000.usdhc: No vqmmc regulator found                         
mmc2: SDHCI controller on 2198000.usdhc [2198000.usdhc] using DMA               
galcore: clk_get gpu3d_clk failed, disable 3d!                                  
Galcore version 5.0.11.41671                                                    
hidraw: raw HID events driver (C) Jiri Kosina                                   
usbcore: registered new interface driver usbhid                                 
usbhid: USB HID core driver                                                     
ashmem: initialized                                                             
usbcore: registered new interface driver snd-usb-audio                          
wm8962 1-001a: Failed to read ID register                                       
wm8962: probe of 1-001a failed with error -5                                    
imx-wm8962 sound: failed to find codec platform device                          
imx-wm8962: probe of sound failed with error -22                                
imx-spdif sound-spdif: snd-soc-dummy-dai <-> 2004000.spdif mapping ok           
NET: Registered protocol family 26                                              
u32 classifier                                                                  
    Actions configured                                                          
Netfilter messages via NETLINK v0.30.                                           
nf_conntrack version 0.5.0 (15932 buckets, 63728 max)                           
ctnetlink v0.93: registering with nfnetlink.                                    
xt_time: kernel timezone is -0000                                               
ip_tables: (C) 2000-2006 Netfilter Core Team                                    
arp_tables: (C) 2002 David S. Miller                                            
Initializing XFRM netlink socket                                                
NET: Registered protocol family 10                                              
mip6: Mobile IPv6                                                               
ip6_tables: (C) 2000-2006 Netfilter Core Team                                   
sit: IPv6 over IPv4 tunneling driver                                            
NET: Registered protocol family 17                                              
NET: Registered protocol family 15                                              
can: controller area network core (rev 20120528 abi 9)                          
NET: Registered protocol family 29                                              
can: raw protocol (rev 20120528)                                                
can: broadcast manager protocol (rev 20120528 t)                                
can: netlink gateway (rev 20130117) max_hops=1                                  
Bluetooth: RFCOMM TTY layer initialized                                         
Bluetooth: RFCOMM socket layer initialized                                      
Bluetooth: RFCOMM ver 1.11                                                      
Bluetooth: BNEP (Ethernet Emulation) ver 1.3                                    
Bluetooth: BNEP filters: protocol multicast                                     
Bluetooth: BNEP socket layer initialized                                        
Bluetooth: HIDP (Human Interface Emulation) ver 1.2                             
Bluetooth: HIDP socket layer initialized                                        
8021q: 802.1Q VLAN Support v1.8                                                 
Key type dns_resolver registered                                                
cpu cpu0: dev_pm_opp_get_opp_count: device OPP not found (-19)                  
dhd_module_init in                                                              
Power-up adapter 'DHD generic adapter'                                          
wifi_platform_bus_enumerate device present 1                                    
mmc0: new high speed SDHC card at address aaaa                                  
mmcblk0: mmc0:aaaa SS08G 7.40 GiB (ro)                                          
 mmcblk0: p1 p2 p3 < p5 p6 p7 p8 p9 > p4                                        
mmcblk0: p4 size 3053190 extends beyond EOD, truncated                          
failed to power up DHD generic adapter, 3 retry left                            
wifi_platform_bus_enumerate device present 0                                    
mmc0: card aaaa removed                                                         
wifi_platform_bus_enumerate device present 1                                    
mmc0: new high speed SDHC card at address aaaa                                  
mmcblk0: mmc0:aaaa SS08G 7.40 GiB (ro)                                          
 mmcblk0: p1 p2 p3 < p5 p6 p7 p8 p9 > p4                                        
mmcblk0: p4 size 3053190 extends beyond EOD, truncated                          
failed to power up DHD generic adapter, 2 retry left                            
wifi_platform_bus_enumerate device present 0                                    
mmc0: card aaaa removed                                                         
wifi_platform_bus_enumerate device present 1                                    
mmc0: new high speed SDHC card at address aaaa                                  
mmcblk0: mmc0:aaaa SS08G 7.40 GiB (ro)                                          
 mmcblk0: p1 p2 p3 < p5 p6 p7 p8 p9 > p4                                        
mmcblk0: p4 size 3053190 extends beyond EOD, truncated                          
failed to power up DHD generic adapter, 1 retry left                            
wifi_platform_bus_enumerate device present 0                                    
mmc0: card aaaa removed                                                         
wifi_platform_bus_enumerate device present 1                                    
mmc0: new high speed SDHC card at address aaaa                                  
mmcblk0: mmc0:aaaa SS08G 7.40 GiB (ro)                                          
 mmcblk0: p1 p2 p3 < p5 p6 p7 p8 p9 > p4                                        
mmcblk0: p4 size 3053190 extends beyond EOD, truncated                          
failed to power up DHD generic adapter, 0 retry left                            
wifi_platform_bus_enumerate device present 0                                    
mmc0: card aaaa removed                                                         
failed to power up DHD generic adapter, max retry reached**                     
snvs_rtc 20cc000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01 03:16:23 )
SW4: disabling                                                                  
wm8962-supply-4v2: disabling                                                    
wm8962-supply-3v15: disabling                                                   
usb_otg1_vbus: disabling                                                        
wlreg_on: disabling                                                             
ALSA device list:                                                               
  #0: imx-spdif                                                                 
Freeing unused kernel memory: 1024K (c1000000 - c1100000)                       
init: init started!                                                             
SELinux:  Android master kernel running Android M policy in compatibility mode.
SELinux:  Permission audit_read in class capability2 not defined in policy.     
SELinux: the above unknown classes and permissions will be denied               
audit: type=1403 audit(11783.610:2): policy loaded auid=4294967295 ses=429496725
audit: type=1404 audit(11783.620:3): enforcing=1 old_enforcing=0 auid=4294967295
init: (Initializing SELinux enforcing took 0.12s.)                              
init: init second stage started!                                                
init: waitpid failed: No child processes                                        
init: property_set("ro.zygote", "zygote32") failed                              
init: (Loading properties from /default.prop took 0.00s.)                       
init: (Parsing /init.environ.rc took 0.00s.)                                    
init: (Parsing /init.usb.rc took 0.00s.)                                        
init: (Parsing init.freescale.usb.rc took 0.00s.)                               
init: (Parsing /init.freescale.rc took 0.01s.)                                  
init: (Parsing /init.usb.configfs.rc took 0.00s.)                               
init: (Parsing /init.zygote32.rc took 0.00s.)                                   
init: (Parsing /init.trace.rc took 0.00s.)                                      
init: (Parsing /init.rc took 0.03s.)                                            
init: SELinux: Could not get canonical path /adb_keys restorecon: No such file .
init: Starting service 'ueventd'...                                             
audit: type=1400 audit(11783.770:4): avc:  denied  { mounton } for  pid=1 comm=0
ueventd: ueventd started!                                                       
init: Waiting for /dev/.coldboot_done...                                        
ueventd: Coldboot took 0.29s.                                                   
init: Waiting for /dev/.coldboot_done took 0.29s.                               
init: Failed to read from /dev/hw_random: No such device                        
init: write_file: Unable to open '/proc/sys/kernel/sched_compat_yield': No suchy
init: write_file: Unable to write to '/dev/cpuctl/cpu.shares': Invalid argument
init: write_file: Unable to open '/proc/sys/abi/swp': No such file or directory
Console: switching to colour dummy device 80x30                                 
init: Failed to read from /dev/hw_random: No such device                        
fs_mgr: Error parsing fs_mgr_options                                            
init: fs_mgr_mount_all returned an error                                        
init: fs_mgr_mount_all returned unexpected error 255                            
file system registered                                                          
init: cannot find '/system/bin/logd', disabling 'logd'                          
init: SELinux: Could not get canonical path /cache/recovery restorecon: No such.
fs_mgr: Error parsing fs_mgr_options                                            
init: (Loading properties from /system/build.prop took 0.00s.)                  
init: (Loading properties from /vendor/build.prop took 0.00s.)                  
init: (Loading properties from /factory/factory.prop took 0.00s.)               
fs_mgr: Error parsing fs_mgr_options                                            
init: unable to read fstab /fstab.freescale: No such file or directory          
init: SELinux: Could not set context for /data:  Read-only file system          
init: cannot find '/system/bin/logd', disabling 'logd'                          
init: cannot find '/system/bin/vold', disabling 'vold'                          
init: Not bootcharting.                                                         
init: SELinux: Could not set context for /data:  Read-only file system          
init: cannot find '/system/bin/tzdatacheck', disabling 'exec 0 (/system/bin/tzd'
init: Unable to open persistent property directory "/data/property": No such fiy
init: cannot find '/system/bin/logd', disabling 'logd'                          
init: cannot find '/system/bin/logd', disabling 'logd-reinit'                   
init: Starting service 'healthd'...                                             
init: cannot find '/system/bin/sh', disabling 'console'                         
binder: 169:169 transaction failed 29189, size 0-0                              
init: cannot find '/system/bin/lmkd', disabling 'lmkd'                          
init: cannot find '/system/bin/servicemanager', disabling 'servicemanager'      
init: cannot find '/system/bin/surfaceflinger', disabling 'surfaceflinger'      
init: write_file: Unable to open '/sys/block/mmcblk0/queue/read_ahead_kb': No sy
init: write_file: Unable to open '/sys/block/mmcblk0/queue/read_ahead_kb': No sy
random: init urandom read with 18 bits of entropy available                     
init: Unable to write persistent property to temp file /data/property/.temp.gZ0y
init: property_set("ro.ril.wake_lock_timeout", "300") failed                    
init: property 'ro.product.manufacturer' doesn't exist while expanding '${ro.pr'
init: cannot expand '${ro.product.manufacturer}' while writing to '/config/usb_'
init: property 'ro.product.model' doesn't exist while expanding '${ro.product.m'
init: cannot expand '${ro.product.model}' while writing to '/config/usb_gadget/'
binder: 169:169 transaction failed 29189, size 0-0                              
binder: 169:169 transaction failed 29189, size 0-0                              
binder: 169:169 transaction failed 29189, size 0-0   

With Best Regards

Joshua

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

2,192件の閲覧回数
mehulshah
Contributor III

did you get any solution for this ? ..if yes then please post it here .

0 件の賞賛
返信