if the MAC57D5xx DRAM controller supporting DDR3?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

if the MAC57D5xx DRAM controller supporting DDR3?

771 次查看
gqzhang
Contributor I

                    A Question about MAC57D5XX

Q:

The MAC57D5xx DRAM controller supporting DDR3?

Does the Expandable Memory Interfaces DDR2 of MAC57D5xx Features can be replaced by Expandable Memory Interfaces DDR3?

 

For example MAC57D5-516DC Evaluation Board – Schematic DDR2 (MT47H64M16NF-25E:M)

 

RE:  ?

 

 

 

 

MAC57D5xx DIS MCUs for Automotive Instrument Cluster

FEATURES
Cortex-A5, 32-bit CPU (Application processor)

Floating point unit (FPU) supporting double-precision floating-point operations

 

Expandable Memory Interfaces

} 2 x Dual Quad SPI serial flash controllers (including Hyper Flash™ support)
} Supports SDR and DDR serial flash
} DRAM controller supporting SDR and DDR2

 

Graphics Features
} Viv ante GC355 GPU supporting Open VG™ 1.1

 

0 项奖励
回复
1 回复

705 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Zhang,

    MAC57D5xx doesn't support DDR3, but SDR or DDR2. So you can't replace DDR2 with DDR3.


Have a great day,
TIC   weidong

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复