if imx27 support WinCE 2013?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

if imx27 support WinCE 2013?

3,020 Views
qu_yandong
Contributor I

Hi, I 'd like to check that if imx27 support WinCE 2013?
I use it for WinCE6 and update it to WinCE7 in last years.

But you know, WinCE 7 is going out of support. So I need do an update or change.

There are lots of devices already sailed and on market. So I only want to do a SW update. No HW update for easy service.

So is there a way to support WinCE2013 on imx27?

Thanks.

Labels (2)
0 Kudos
Reply
3 Replies

2,913 Views
qu_yandong
Contributor I

Hi, 

Thanks for your feed back.

Do you mean NXP/ Freescale are working on the WinCE2013 for iMX27?

And is there a timeline for that?

 

I mean that the WinCE2013 has been come out for 6 years. 

I can understand that iMX27 is too old or slow for Wince2013.

So if there will not be a update package for iMX27 is understandable.

Please just let me know if there is a update for this.

Thanks.

0 Kudos
Reply

2,913 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Kevin,

Sorry, Unfortunately Wince 2013 is not done for MX27, there is not much effort in MX27 since it will end soon.

Regards

0 Kudos
Reply

2,913 Views
qu_yandong
Contributor I

Hi, 

Thanks for your feed back.

Do you mean NXP/ Freescale are working on the WinCE2013 for iMX27?

And is there a timeline for that?

I mean that the WinCE2013 has been come out for 6 years. 

I can understand that iMX27 is too old or slow for Wince2013.

So if there will not be a update package for iMX27 is understandable.

Please just let me know if there is a update for this.

Thanks.

0 Kudos
Reply