if I want to add/delete qt assembly such as linuxfb, what should I do?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

if I want to add/delete qt assembly such as linuxfb, what should I do?

1,332 Views
cilymo
Contributor I

if I want to add/delete qt assembly such as linuxfb, what should I do?

My BSP is 4.1.15.

Labels (2)
0 Kudos
Reply
1 Reply

1,273 Views
igorpadykov
NXP Employee
NXP Employee

Hi cily

please refer to fsl-image-qt5 in Table 1. Freescale Yocto project images attached Yocto Guide

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply