icmp_seq=1 Destination Host Unreachable

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

icmp_seq=1 Destination Host Unreachable

24,791件の閲覧回数
santhosh2
Contributor IV

Hi,

I am unable to ping the host through i.mx8mm board and also i have checked on the scope that packets are not getting transmitted from Processor TX/RX pin. what is the configuration that iam missing, i am unable to ping from uboot as well as from the linux kernel

root@imx8mmevk:~# ifconfig
eth0      Link encap:Ethernet  HWaddr 02:01:02:03:04:05  
          inet addr:192.168.36.126  Bcast:192.168.36.255  Mask:255.255.255.0
          inet6 addr: fe80::1:2ff:fe03:405/64 Scope:Link
          UP BROADCAST RUNNING MULTICAST DYNAMIC  MTU:1500  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000
          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

lo        Link encap:Local Loopback  
          inet addr:127.0.0.1  Mask:255.0.0.0
          inet6 addr: ::1/128 Scope:Host
          UP LOOPBACK RUNNING  MTU:65536  Metric:1
          RX packets:2651 errors:0 dropped:0 overruns:0 frame:0
          TX packets:2651 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000
          RX bytes:191868 (187.3 KiB)  TX bytes:191868 (187.3 KiB)

root@imx8mmevk:~# route -n
Kernel IP routing table
Destination     Gateway         Genmask         Flags Metric Ref    Use Iface
0.0.0.0         192.168.36.1    0.0.0.0         UG    0      0        0 eth0
0.0.0.0         0.0.0.0         0.0.0.0         U     0      0        0 eth0
169.254.0.0     0.0.0.0         255.255.0.0     U     0      0        0 eth0
192.168.36.0    0.0.0.0         255.255.255.0   U     0      0        0 eth0

root@imx8mmevk:~# [  560.262908] fec 30be0000.ethernet eth0: Graceful transmit stop did not complete!
[  560.270335] fec 30be0000.ethernet eth0: Link is Down
[  560.324080] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[  561.287018] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
[  561.294869] fec 30be0000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx

root@imx8mmevk:~# ping 192.168.36.136
PING 192.168.36.136 (192.168.36.136) 56(84) bytes of data.
[  570.502790] random: crng init done
[  570.506204] random: 7 urandom warning(s) missed due to ratelimiting
From 192.168.36.126 icmp_seq=1 Destination Host Unreachable
From 192.168.36.126 icmp_seq=2 Destination Host Unreachable
From 192.168.36.126 icmp_seq=3 Destination Host Unreachable
From 192.168.36.126 icmp_seq=4 Destination Host Unreachable
From 192.168.36.126 icmp_seq=5 Destination Host Unreachable
From 192.168.36.126 icmp_seq=6 Destination Host Unreachable
From 192.168.36.126 icmp_seq=7 Destination Host Unreachable
From 192.168.36.126 icmp_seq=8 Destination Host Unreachable
From 192.168.36.126 icmp_seq=9 Destination Host Unreachable
^C
--- 192.168.36.136 ping statistics ---
10 packets transmitted, 0 received, +9 errors, 100% packet loss, time 9205ms
pipe 4

0 件の賞賛
返信
5 返答(返信)

23,207件の閲覧回数
Popov_Vasil
Contributor II

Hey!
I have the same problem, however, i'm trying to ping using WiFi connection. The board is i.MX8M Plus EVK, release is: LF5.10.35_2.0.0. The route table and the output of ifconfig are presented inside the image.

PING 192.168.1.127 (192.168.1.127) 56(84) bytes of data.
From 192.168.1.245 icmp_seq=1 Destination Host Unreachable
From 192.168.1.245 icmp_seq=2 Destination Host Unreachable
From 192.168.1.245 icmp_seq=3 Destination Host Unreachable

 

0 件の賞賛
返信

24,641件の閲覧回数
b36401
NXP Employee
NXP Employee

It seems you have wrong routing table.
There should not be more than one default gateways (rules with 0.0.0.0 destination).
Please remove this one:
0.0.0.0 0.0.0.0 0.0.0.0 U 0 0 0 eth0

0 件の賞賛
返信

24,643件の閲覧回数
santhosh2
Contributor IV

HI victor,

I used below command but its not getting removed, Please advice the command

root@imx8mmevk:~# route add -net 0.0.0.0 gw 0.0.0.0 dev eth0

root@imx8mmevk:~# route -n
Kernel IP routing table
Destination     Gateway         Genmask         Flags Metric Ref    Use Iface
0.0.0.0         192.168.36.1    0.0.0.0         UG    0      0        0 eth0
0.0.0.0         0.0.0.0         0.0.0.0         U     0      0        0 eth0
169.254.0.0     0.0.0.0         255.255.0.0     U     0      0        0 eth0
192.168.36.0    0.0.0.0         255.255.255.0   U     0      0        0 eth0

0 件の賞賛
返信

24,643件の閲覧回数
santhosh2
Contributor IV

Sorry, there is a Typo error in the command in my perious reply,

I used below command but its not getting removed, Please advice the command

root@imx8mmevk:~# route del -net 0.0.0.0 gw 0.0.0.0 dev eth0

root@imx8mmevk:~# route -n
Kernel IP routing table
Destination     Gateway         Genmask         Flags Metric Ref    Use Iface
0.0.0.0         192.168.36.1    0.0.0.0         UG    0      0        0 eth0
0.0.0.0         0.0.0.0         0.0.0.0         U     0      0        0 eth0
169.254.0.0     0.0.0.0         255.255.0.0     U     0      0        0 eth0
192.168.36.0    0.0.0.0         255.255.255.0   U     0      0        0 eth0

0 件の賞賛
返信

24,643件の閲覧回数
b36401
NXP Employee
NXP Employee

Please try to run "route del -net 0.0.0.0" twice to remove both lines and then add one right.

0 件の賞賛
返信