icecast audio streaming on android 5.1 default browser

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

icecast audio streaming on android 5.1 default browser

2,454 Views
yenchao
Contributor IV

Hi,

I'm working on android 5.1 with imx6dl for playing audio streaming  from a icecast server.

When I enter below url  and click start button by android default browser.

http://202.212.210.163/test/abe_autoplay/audio0511.html

It will show some error messages as follows.

----------------------------------

I/OMXPlayer( 191): Loading content: http://202.212.210.163:8000/ices
I/OMXPlayer( 191): LEVEL: 1 FUNCTION: MediaTypeInspect LINE: 1965
I/OMXPlayer( 191): Can't inspect media content type by subfix.
E/SQLiteLog( 1175): (284) automatic index on sqlite_sq_AF150D80(url)
I/OMXPlayer( 191): LEVEL: 1 FUNCTION: GetContentLength LINE: 115
I/OMXPlayer( 191): GetContentLength url_seek AVSEEK_SIZE fail
PU: Power-off latency exceeded, new value 25667 ns
I/OMXPlayer( 191): transfer_func data timeout.
I/OMXPlayer( 191): LEVEL: 1 FUNCTION: Seek LINE: 277
I/OMXPlayer( 191): HttpsProtocol::Seek() fail, ret -1, request 5120
I/OMXPlayer( 191): server seekable: 1
I/OMXPlayer( 191): HttpsProtocol::Read() terminated
I/OMXPlayer( 191): file size: 0, buffer size : 0

I/OMXPlayer( 191): transfer_func data timeout.
I/OMXPlayer( 191): LEVEL: 1 FUNCTION: GetContentLength LINE: 115
I/OMXPlayer( 191): GetContentLength url_seek AVSEEK_SIZE fail
I/OMXPlayer( 191): server seekable: 0
I/OMXPlayer( 191): transfer_func data timeout.
I/OMXPlayer( 191): LEVEL: 1 FUNCTION: Seek LINE: 277
I/OMXPlayer( 191): HttpsProtocol::Seek() fail, ret -1, request 0
I/OMXPlayer( 191): LEVEL: 1 FUNCTION: GetContentLength LINE: 115
I/OMXPlayer( 191): GetContentLength url_seek AVSEEK_SIZE fail
I/OMXPlayer( 191): LEVEL: 1 FUNCTION: GetContentLength LINE: 115
I/OMXPlayer( 191): GetContentLength url_seek AVSEEK_SIZE fail
I/OMXPlayer( 191): LEVEL: 1 FUNCTION: GetContentLength LINE: 115
I/OMXPlayer( 191): GetContentLength url_seek AVSEEK_SIZE fail
I/OMXPlayer( 191): LEVEL: 1 FUNCTION: GetContentLength LINE: 115
I/OMXPlayer( 191): GetContentLength url_seek AVSEEK_SIZE fail
I/OMXPlayer( 191): LEVEL: 1 FUNCTION: GetContentLength LINE: 115
I/OMXPlayer( 191): GetContentLength url_seek AVSEEK_SIZE fail
I/OMXPlayer( 191): LEVEL: 1 FUNCTION: GetContentLength LINE: 115
I/OMXPlayer( 191): GetContentLength url_seek AVSEEK_SIZE fail
I/OMXPlayer( 191): LEVEL: 1 FUNCTION: GetContentLength LINE: 115
I/OMXPlayer( 191): GetContentLength url_seek AVSEEK_SIZE fail

-----------------------------------------------

If I install and use chrome browser to play this audio streaming then everything goes well.

Does anyone know how to fix this issue?

Any advice and suggestion would be greatly appreicated.

Thx

Yen

Labels (4)
0 Kudos
Reply
2 Replies

2,261 Views
diegoadrian
NXP Employee
NXP Employee

Hello, 

I do not know if you are still having a problem.

If yes, can you please tell me which command are you using to stream the Audio? or, are you using an application?

Best Regards,

Diego.

0 Kudos
Reply

2,261 Views
yenchao
Contributor IV

Hi Diego,

The problem is not solved.

I'm using android 5.1 default browser.

Thx

Yen

0 Kudos
Reply