iMx8 Ethernet MAC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMx8 Ethernet MAC

2,698 Views
deepaknath
Contributor I

Does the Ethernet_PHY support the following :

1. Capable of Supporting QoS

2.  Capable of prioritizing messages so that higher priority messages have lower latency.

3.  Can the Ethernet Interface be configured with unique MAC address?

0 Kudos
Reply
2 Replies

2,436 Views
b36401
NXP Employee
NXP Employee
0 Kudos
Reply

2,436 Views
b36401
NXP Employee
NXP Employee

i.MX8M processors are not able to separate Ethernet packets for several different queues.
So they do not support QoS and prioritizing.
Please note that i.MX series are more multimedia than networking processors.

As for MAC address you can change it.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply