iMx8 Ethernet MAC

cancel
Showing results for 
Search instead for 
Did you mean: 

iMx8 Ethernet MAC

419 Views
deepaknath
Contributor I

Does the Ethernet_PHY support the following :

1. Capable of Supporting QoS

2.  Capable of prioritizing messages so that higher priority messages have lower latency.

3.  Can the Ethernet Interface be configured with unique MAC address?

0 Kudos
2 Replies

157 Views
b36401
NXP TechSupport
NXP TechSupport
0 Kudos

157 Views
b36401
NXP TechSupport
NXP TechSupport

i.MX8M processors are not able to separate Ethernet packets for several different queues.
So they do not support QoS and prioritizing.
Please note that i.MX series are more multimedia than networking processors.

As for MAC address you can change it.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos