iMx7 tamper

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMx7 tamper

2,087件の閲覧回数
lucas_lin
Contributor I

Hi,


I have a new project and the SOC is iMX7s.
I need to implement tamper detection function.

According to the "i.MX 7Solo Applications Processor Reference Manual" in section "3.1.4.2 Tamper Detection", it descriptors the tamper detection function need an always-ON power supply (coincell battery) should be present in the system.

But my project has size limitation and can't support an always-ON power supply (coincell battery).
My question is if there isn't exist an always-ON power supply, how to implement tamper detection function in my project?

Thank you.

ラベル(3)
0 件の賞賛
返信
1 返信

1,983件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Lucas

>My question is if there isn't exist an always-ON power supply,

>how to implement tamper detection function in my project?

seems this is not feasible with i.MX7S/D as its tamper functionality requires

always-on power supply.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------