Booting from SD card

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Booting from SD card

1,742件の閲覧回数
aabhishekoct18
Contributor III

Hi Team 

We made our options  to boot  from SD card during internal Boot, Can you please confirm when clock should come.Does it samples  CD  pin , then clock  will  come  after  ensuring SD  card is there or  something else  ? What is  sequence  of  whole  process?. 

How handshaking happen between  SD card and processor ? 

ラベル(1)
0 件の賞賛
返信
1 返信

1,680件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Abhishek

sd boot sequence is described in Figure 8-10. Expansion device boot flow,

sect.8.5.3.4 IOMUX configuration for SD/MMC

i.MX 6Solo/6DualLite Applications Processor Reference Manual

>Does it samples  CD  pin , then clock  will  come  after  ensuring SD  card ..

right.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信