iMx6UL Rx485 Mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMx6UL Rx485 Mode

2,125件の閲覧回数
prabhatkumar
Contributor II

It is not clear to me from  datasheet about the polarity of the CTS_B pin when set in RS485 mode? Does switching from full duplex to half duplex or vice versa affects the direction of CTS_B pin?

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,718件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Prabhat

one can check example on p.3162 i.MX6UL Reference Manual:

Set software flow control (CTS pin is controlled by UCR2[12] ),

from sect.53.15.4 UART Control Register 2 (UARTx_UCR2)

0 The CTS_B pin is high (inactive)
1 The CTS_B pin is low (active)

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6ULRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------