iMx6UL Rx485 Mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMx6UL Rx485 Mode

2,122 Views
prabhatkumar
Contributor II

It is not clear to me from  datasheet about the polarity of the CTS_B pin when set in RS485 mode? Does switching from full duplex to half duplex or vice versa affects the direction of CTS_B pin?

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,715 Views
igorpadykov
NXP Employee
NXP Employee

Hi Prabhat

one can check example on p.3162 i.MX6UL Reference Manual:

Set software flow control (CTS pin is controlled by UCR2[12] ),

from sect.53.15.4 UART Control Register 2 (UARTx_UCR2)

0 The CTS_B pin is high (inactive)
1 The CTS_B pin is low (active)

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6ULRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------