iMx6 dual IPU error IPU_INT_STAT_10 using CSC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMx6 dual IPU error IPU_INT_STAT_10 using CSC

3,438件の閲覧回数
ed_nash
Contributor III

Hi-

Below is a small (< 100lines) test program which produces IPU_INT_STAT_10 = 0x0008000.

The program just converts color space between two buffers.

There is no other activity at the time.

The display is a 1200 X 800 RGB888 ldb display, but is only showing the boot image - no video, no gstreamer.

Kernel is 3.0.35.

Any ideas?

Thanks in advance. Program follows

#define WIDTH 120

//0

#define HEIGHT 80

//0

#define INPUT_FMT (IPU_PIX_FMT_UYVY)

#define OUTPUT_FMT (IPU_PIX_FMT_RGB565)

#define BPP 2

#define BUF_SIZE (WIDTH * HEIGHT * BPP)

static int fd_ipu;

static struct ipu_task task;

static uint8_t *inbuf, *outbuf;

static void init_task(void)

{

  memset(&task, 0, sizeof(task));

  task.input.width = WIDTH;

  task.input.height = HEIGHT;

  task.input.format = INPUT_FMT;

  task.output.width = WIDTH;

  task.output.height = HEIGHT;

  task.output.format = OUTPUT_FMT;

}

static uint8_t *ipu_allocate(dma_addr_t *paddr)

{

  *paddr = BUF_SIZE;

  if(ioctl(fd_ipu, IPU_ALLOC, paddr))

  {

  perror("IPU_ALLOC");

  return NULL;

  }

  return mmap(0, BUF_SIZE, PROT_READ | PROT_WRITE, MAP_SHARED, fd_ipu, *paddr);

}

static void ipu_free(dma_addr_t *paddr)

{

  munmap((void *)*paddr, BUF_SIZE);

  if(ioctl(fd_ipu, IPU_FREE, paddr))

  {

  perror("IPU_FREE");

  return;

  }

}

int main(int argc, char *argv[])

{

  int i;

  fd_ipu = open("/dev/mxc_ipu", O_RDWR, 0);

  if (fd_ipu < 0)

  {

  perror("/dev/mxc_ipu");

  return 1;

  }

  init_task();

  inbuf = ipu_allocate(&task.input.paddr);

  outbuf = ipu_allocate(&task.output.paddr);

  memset(inbuf, 128, BUF_SIZE);

  for(i=0; i<1; i++)

  {

  int err = ioctl(fd_ipu, IPU_QUEUE_TASK, &task);

  if (err)

  perror("IPU_QUEUE_TASK");

  else

  printf("IPU_QUEUE_TASK success\n");

  }

  ipu_free(&task.input.paddr);

  ipu_free(&task.output.paddr);

  close(fd_ipu);

printf("Done\n");

return 0;

}

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,628件の閲覧回数
ed_nash
Contributor III

Some more info - if I comment out the ldb display in the board file there is no error so there must be some kind of conflict.

0 件の賞賛
返信

2,628件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ed

IPU_INT_STAT_10 =0x00080000" , that is bit 19 of IPU_INT_STAT_10 is DI0_SYNC_DISP_ERR.

This bit is set when there's an error, usually as result of data starvation when

data that should be sent to display is not available in IPUs internal FIFO.

It means that the IPU encounters the data starvation, that is, it can not

get data sometimes from memory.

Most probable cause for this issue is big load on the DDR memory bus.

You may adjust this by decreasing memory access loading (for example

decreasing frame rate) or by optimizing your application (for example increasing

operating frequencies).

For csc example one can also look at

ipu-examples/csc_ex1.c at master · rogeriorps/ipu-examples · GitHub

Best regards

igor

0 件の賞賛
返信

2,628件の閲覧回数
ed_nash
Contributor III

Thanks for the response Igor, but I think it's something else going on.

I did the test in an attempt to isolate the issue. So there was no other activity in the system. I was not capturing video or displaying anything other than the boot logo that was already in the framebuffer. and there was no other programs running.

Also, I used a really small buffer size for my test - 120 x 80.

I did look at Rogerio's examples - that's where I pulled code to make my test program.

Any other thoughts?

Thanks again.

0 件の賞賛
返信

2,628件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ed

I would suggest to run rogeriorps/ipu-examples

on Demo image

L3.0.35_4.1.0_DEMO_IMAGE_BSP

Also one can look at SDK CSC example i.MX 6Series Platform SDK : Bare-metal SDK

Best regards

igor

0 件の賞賛
返信