iMx6 Processor ID

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMx6 Processor ID

2,117 Views
venkatesh_compa
Contributor I

Hi,

Would like to know i.MX6 process_id <device_unique> 64-bit UID is unique? whether each processor will have unique ID  that can be guaranteed?

Part Number# MCIMX6G2ABM05AB

For example# if i procure 50 pieces of above mention part number, whether i can get different unique process ID for these items.

Regards,

Venkatesh. C.S

Labels (1)
0 Kudos
Reply
3 Replies

2,007 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  yes, the i.MX6 fuse UNIQUE_ID[63:0] provides  unique ID for each i.MX6 device.

 

Have a great day,

Yuri

 

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

 

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 Kudos
Reply

2,007 Views
venkatesh_compa
Contributor I

Hi Yuri,

Thanks for your reply, to make it clear.

Let say if device 1[MCIMX6G2ABM05AB] has 0x11,0x12,0x13,0x14,0x15,0x16,0x17,0x18

So device2[MCIMX6G2ABM05AB] shall have unique value other than above value?

Regards,

Venkatesh.C.S

0 Kudos
Reply

2,007 Views
Yuri
NXP Employee
NXP Employee

Your understanding is correct.

~Yuri.

0 Kudos
Reply