iMXRT1176 flashing error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMXRT1176 flashing error

2,675 次查看
Aparna
Contributor I

Hi,

We designed a custom board with iMXRT1176, and a W25Q512NWEIM serial flash. When trying to upload the hello_world application, error occurs in one board. Also I tried the option "link application to ram" still it fails. Please suggest a solution to overcome the issue.

error.png

error occurs in "link application to ram" option

error_ link to ram.png

 

 

0 项奖励
回复
3 回复数

2,666 次查看
PabloAvalos
NXP TechSupport
NXP TechSupport

Hi @Aparna 

 

Thanks a lot for using our community to reach our technical support. I really appreciate your patience.

 

Firstly, I see that you opened other two threads about the same issue that you are having, so what about if everything is managed on this one? it would be my pleasure to assist you in all the questions you have regarding your concern right here.

 

Then, checking the issue you are experimenting, I would like to suggest you to check all the points and hints that are posted on this web site to see if you find the solution for your debugging issues: https://mcuoneclipse.com/2014/11/03/debugging-failure-check-list-and-hints/

After checking the post, hope you may find the solution to your problem, but if not, please do not hesitate to ask me or tell me your comments.

 

Highly appreciated it. Thank you.

 

Best Regards.
Pablo Avalos.

0 项奖励
回复

2,628 次查看
Aparna
Contributor I

Hi Pablo

Thanks for your support.

I have checked all the points that you were shared. 

Actually, I faced these flashing and debugging errors recently in my working boards. Initially boards were working without any flash or debug issue. I have checked all the voltages of IMXRT1176, everything is within the limit.

Also checked the power sequencing of board, it is as per the recommendation.

Could you please help to solve this issue.

0 项奖励
回复

2,622 次查看
PabloAvalos
NXP TechSupport
NXP TechSupport

Hi @Aparna 

 

Thanks a lot for letting me know an update.

 

in order to do another test, do you think you may try to do a mass erase to your board? This is for discard your board is not bricked, because it is too weird that after following the suggestions and checking the correct voltages, you still cannot flash or debug your boards as you could before.

 

A suggestion is to use the MCU Boot Utility for your RT1170. Please check this link to download it:

https://github.com/JayHeng/NXP-MCUBootUtility

And here there is a brief guide to connect successfully your board:

https://community.nxp.com/t5/i-MX-RT/i-MX-RT1170-with-MCU-Boot-Utility/td-p/1303418

 

Please let me know an update and if it is possible, some screenshots that might tell me the error log you are obtaining besides the ones that you already sent. Also let me know if you need more help. I highly appreciate it.

 

Thanks in advance.
Best Regards.
Pablo Avalos.

0 项奖励
回复