iMXRT1172 SNVS bank -ON/OFF pin function query

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMXRT1172 SNVS bank -ON/OFF pin function query

跳至解决方案
1,140 次查看
vihang_vinayak
Contributor II

Hi,

We are using the iMXRT1172 in one of the battery application project. In my project to put iMXRT1172 in SNVS mode we are using the ONOFF pin (Ball no: U10) 

We just want to know if the ONOFF pin is independent of the execution code incase if the firmware gets stuck internally. I should be able to use the functionality of emergency off using the ONOFF pin.

Please confirm that the ONOFF pin is independent of the execution of code.

Quick response is appreciated.

Best Regards,

Vihang Waze

Design Engineer

Tata Elxsi Limited

0 项奖励
回复
1 解答
1,121 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Yes, the ONOFF pin is independent of the execution of code.

 

BR,

Edwin.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,118 次查看
vihang_vinayak
Contributor II

Thank you Edwin for the confirmation

0 项奖励
回复
1,122 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Yes, the ONOFF pin is independent of the execution of code.

 

BR,

Edwin.

0 项奖励
回复