iMX93 linux prebuilt image and flashing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX93 linux prebuilt image and flashing

Jump to solution
4,483 Views
KHL
Contributor I

Hi,

I dowloaded iMX93 evk prebuilt images "LF_v6.1.1_1.0.0_images_IMX93EVK", there are lots of dtb, bin files in the package. I wish to flash back the default images, which image should I flash and how ?

I tried using uuu to flash "imx-image-full-imx93evk.tar.zst", but an error pops up as per below 

KHL_1-1685623336248.png

I tried switch to using a linux host machine, the uuu outcome remains. What went wrong ?

Thanks.

 

0 Kudos
Reply
1 Solution
4,468 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

I hope you are doing well.

I suggest you use the next command with the board on USB serial download mode.

uuu -b emmc_all imx-image-full-imx93evk.wic

Best regards.

Jorge.

View solution in original post

0 Kudos
Reply
2 Replies
4,469 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

I hope you are doing well.

I suggest you use the next command with the board on USB serial download mode.

uuu -b emmc_all imx-image-full-imx93evk.wic

Best regards.

Jorge.

0 Kudos
Reply
4,455 Views
KHL
Contributor I

Thank you. It works.

0 Kudos
Reply